Part Number: AM625
Team,
A customer of mine noted that pixelclk of AM62 DPI is active, even if DPI is not used. The only use a OLDI display connected to VP1. DPI is NOT activated in the Linux kernel. Also enable bits of registers VP2_CONTROL and VP1_CONTROL are set correctly. The measure 170 MHz on pixelclk of VP2 (DPI).
How can this be disabled? What about the DPIENABLE bit, which is present in both control registers? There is not detailed description.
Thanks,
Robert