Part Number: AM625
Hi Support team.
I have a few questions about the AM625 CPU for which I can't find a clear answer in any document provided on the product's page.
My questions are related to the Display outputs.
In the datasheet it is mentioned the following:
Multimedia:
• Display subsystem
– Dual display support
– 1920x1080 @ 60fps for each display
– 1x 2048x1080 + 1x 1280x720
– Up to 165 MHz pixel clock support with
Independent PLL for each display
– OLDI (4 lanes LVDS - 2x) and DPI (24-bit RGB
LVCMOS)
As I understand from the datasheet, the AM625 CPU has one 2-channel LVDS interface and one 24-bit DPI (parallel) display interface:
- What is the maximum resolution at a 60Hz refresh rate for the LVDS display when a single LVDS channel is used?
- What is the maximum resolution at a 60Hz refresh rate for the LVDS display when both LVDS channels are used?
- What is the maximum resolution at a 60Hz refresh rate for the two LVDS displays connected to the separate LVDS channels?
- What is the maximum resolution at a 60Hz refresh rate for the 24-bit DPI (parallel) display?
- Is it possible to use LVDS and DPI displays simultaneously? What is the maximum resolution at a 60Hz in Dual display configuration?