This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62: display output

Guru 10245 points

Part Number: SK-AM62

Hi Support Team,

I have questions about the SK-AM62 display output.

Q1. There are HDMI and LVDS IFs. If I connect a display to each of them, can I confirm "2 independent displays at FHD@60fps"?

Q2: If the answer to Q1 is "yes," please provide the specifications of each display that can be checked.
Also, please provide the display you actually used for evaluation or the display you recommend.

Q3: If the answer to Q1 is not "possible," please provide the display specifications that can be checked on the reference board.
Also, if "independent display of two screens at FHD@60fps" is possible with a conversion board, etc., please provide us with an example configuration.

Best regards,
Kanae