This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Python Code Module Integration with the Vision Application

Part Number: TDA4VM

Dear Sir,

I have a post-processing module written in Python code, Is there any way or tool to integrate it with my existing vision application as custom kernel or Node?

Thanks and Regards,

Vyom Mishra

  • Hi Vyom,

    You could either create a full application using the python script as shown in ${PSDKRA}/tiovx/tutorial/ch03_graph/vx_tutorial_graph_image_gradients_pytiovx_uc.py
    or

    create a node using the python script as shown in ${PSDKRA}/vision_apps/kernels/srv/scripts/kernel_gpu_srv.py
    and then use the node api into your existing application.

    These are the two ways supported in the SDK.

    Regards,

    Nikhil