This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: MCU1_0 crash

Part Number: TDA4VM

Hello TI Expert.

I also meet the similar issue on my HS TDA4VM.MCU1_0 no response.after investigattion,Data Abort occur,then while(1) crash.

because the reproduce way is:

1.power on, TDA4 chip temperature high

2.power off

3.wait more than 5mins,about 5~10mins

4.power on

5.issue occur some times.

  note:if i press some key in A72 uart window which let A72 stop at uboot,then mcu1_0 not crash...

          it looks that SCI ineraction with other cores is the issue trigger condtion.

becasue the operation is power on->off->on............. I can NOTuse debugger

Question:

Can you give me some advise for investigate this issue?

log as following:

: rproc started
xauto: jumping linux
[ 0.224948] remoteproc remoteproc16: rsc table ver invalid 7ffffefd, ignored
[ 1.249162] ti-sci 44083000.dmsc: Mbox timedout in resp(caller: ti_sci_cmd_get_device_exclusive+0x18/0x28)
[ 1.258808] ti-sci 44083000.dmsc: Mbox send fail -110
NOTICE: BL31: v2.5(release):08.00.00.002-dirty
NOTICE: BL31: Built : 02:14:08, Aug 9 2023

U-Boot SPL 2021.01 (Aug 09 2023 - 02:14:46 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.9.1--v2021.09a (Terrific Lla')
xauto: boot
Loading Environment from nowhere... OK
xauto: mem bootslot b
xauto: rproc started
xauto: jumping linux
[ 1.248643] ti-sci 44083000.dmsc: Mbox timedout in resp(caller: ti_sci_cmd_dev_is_on+0x48/0xa8)
[ 1.257336] ti-sci 44083000.dmsc: Mbox send fail -110
[ 1.262377] platform 41400000.r5f: failed to get initial state, mode cannot be determined, ret = -110
[ 1.271836] k3_r5_rproc bus@100000:bus@28380000:r5fss@41000000: k3_r5_cluster_rproc_init failed, ret = -110
NOTICE: BL31: v2.5(release):08.00.00.002-dirty
NOTICE: BL31: Built : 02:14:08, Aug 9 2023

U-Boot SPL 2021.01 (Aug 09 2023 - 02:14:46 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.9.1--v2021.09a (Terrific Lla')
xauto: boot
Loading Environment from nowhere... OK
xauto: mem bootslot a
xauto: rproc started
xauto: jumping linux
[ 0.217377] remoteproc remoteproc16: rsc table ver invalid 7ffffefd, ignored
[ 1.249161] ti-sci 44083000.dmsc: Mbox timedout in resp(caller: ti_sci_cmd_clk_is_on+0x48/0xa8)
[ 1.257855] ti-sci 44083000.dmsc: Mbox send fail -110
[ 1.262897] ti-sci-clk 44083000.dmsc:clocks: is_prepared failed for dev=297, clk=13, ret=-110
NOTICE: BL31: v2.5(release):08.00.00.002-dirty
NOTICE: BL31: Built : 02:14:08, Aug 9 2023

U-Boot SPL 2021.01 (Aug 09 2023 - 02:14:46 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.9.1--v2021.09a (Terrific Lla')
xauto: boot
Loading Environment from nowhere... OK
xauto: mem bootslot b
xauto: rproc started
xauto: jumping linux
[ 0.219133] remoteproc remoteproc16: rsc table ver invalid 7ffffefd, ignored
[ 1.249129] ti-sci 44083000.dmsc: Mbox timedout in resp(caller: ti_sci_cmd_get_device_exclusive+0x18/0x28)
[ 1.258772] ti-sci 44083000.dmsc: Mbox send fail -110
NOTICE: BL31: v2.5(release):08.00.00.002-dirty
NOTICE: BL31: Built : 02:14:08, Aug 9 2023

U-Boot SPL 2021.01 (Aug 09 2023 - 02:14:46 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.9.1--v2021.09a (Terrific Lla')
xauto: boot
Loading Environment from nowhere... OK