This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA821U: Please help analyze the issue of network connectivity

Part Number: DRA821U

Hi TI,

Our client has two cars that occasionally experience network connectivity during testing.

TI SDK version: pdk_J7200_08_00_00_37.

Hardware connection as shown in the figure: 821 is connected to TC397 through switch, and to PC through phy dp83tg720s.

Network blockage refers to the situation where both TC397 and PC cannot ping 821, and executing ifconfig/ping within 821 will result in stuck output without any information.
Captured slog、core and tarcelog as attached.
We have contacted QNX to assist with the analysis, and QNX suspects that it is cpsw_start() function is blocked, QNX feedback is shown in the screenshot.

Please help analyze whether the problem is related to cpsw_start() ?
Or are there any other directions for investigation?

5545.log.zip

Thanks