Part Number: AM625
I am working on custom board base on am625, where third party did a u-boot port using TI SDK 08.05.00.00 and provide the u-boot changes.
I am trying to build u-boot out of the box using the Link.
we are using yocto meta-ti which is on version 08.06.00.003. Before migrating to yocto i am building u-boot out of the box by porting u-boot changes provided for 08.05.00.00.
so i checked out ti-u-boot, k3-image-gen, k3-image-gen on same branch i.e 08.06.00.003. As i am getting build with ATF, so i am using ATF & OPTEE prebuild binaries from ti sdk 08.06.00.042.
variables export
====================
2025  export TI_SECURE_DEV_PKG=/home/siva-test/ti-processor-sdk-linux-rt-am62xx-evm-08.06.00.42/board-support/core-secdev-k3/
 2026  export UBOOT_DIR=/home/siva-test/MUBOOT/ti-u-boot/
 2027  export K3IG_DIR=/home/siva-test/MUBOOT/k3-image-gen/
 2028  export TFA_DIR=/home/siva-test/ti-processor-sdk-linux-rt-am62xx-evm-08.06.00.42/board-support/prebuilt-images/
 2030  export OPTEE_DIR=/home/siva-test/ti-processor-sdk-linux-rt-am62xx-evm-08.06.00.42/board-support/prebuilt-images/
 2031  export SYSFW_DIR=/home/siva-test/MUBOOT/ti-linux-firmware/
 2032  export DMFW_DIR=/home/siva-test/MUBOOT/ti-linux-firmware/ti-dm/
 2035  export DMFW_DIR=/home/siva-test/MUBOOT/ti-linux-firmware/ti-dm/am62xx/
 2039  export PATH=$PATH:PATH_TO_SDK/linux-devkit/sysroots/x86_64-arago-linux/usr/bin
 2040  export PATH=$PATH:/home/siva-test/ti-processor-sdk-linux-rt-am62xx-evm-08.06.00.42/linux-devkit/sysroots/x86_64-arago-linux/usr/bin
 2047  export SYSFW_DIR=/home/siva-test/MUBOOT/ti-linux-firmware/ti-sysfw     
Build
===================
2036  make clean
 2038  make clean
 2041  make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabihf- am62x_evm_r5_defconfig O=$UBOOT_DIR/out/r5
 2042  make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabihf- O=$UBOOT_DIR/out/r52050  make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabihf- SOC=am62x SOC_TYPE=gp SBL=$UBOOT_DIR/out/r5/spl/u-boot-spl.bin SYSFW_DIR=$SYSFW_DIR
 2053  make ARCH=arm CROSS_COMPILE=aarch64-none-linux-gnu- am62x_evm_a53_defconfig O=$UBOOT_DIR/out/a53
 2056  make ARCH=arm CROSS_COMPILE=aarch64-none-linux-gnu- am62x_evm_a53_defconfig O=$UBOOT_DIR/out/a53
 2057  make ARCH=arm CROSS_COMPILE=aarch64-none-linux-gnu- ATF=$TFA_DIR/bl31.bin TEE=$OPTEE_DIR/bl32.bin  DM=$DMFW_DIR/ipc_echo_testb_mcu1_0_release_strip.xer5f O=$UBOOT_DIR/out/a53
u-boot binaries:
===================
./out/r5/tiboot3.bin
./out/a53/tispl.bin
./out/a53/u-boot.img
after flashing the binaries to emmc, board is not booting up. Not getting any output on serial console.