This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: AM625 eFuse configuration

Part Number: AM625
Other Parts Discussed in Thread: AM623,

I'm working on the Computer on Module design based on the AM625 / AM623 SoCs.

I didn't find in the datasheet and reference manual clear information about the eFuse feature.

Which peripherals can be configured with the eFuse?

Is the following sentence correct?

One-Time Programmable eFuses may be used to configure the MAC address, security
keys, device ID, or disable peripherals/features such as JTAG, UARTs.
Recovery mode may be disabled through eFuses, preventing a malicious actor to quickly swap the module’s
image. When using secure boot, even an eMMC replacement is not capable of changing the keys
to validate a malicious image, as security keys are stored in eFuses.