Part Number: AM62A7-Q1
Hi Expert,
Customer DesaySV feedback that the AM62A will reset when the temperature goes up around 122C. I let customer print the VTM value per 0.5s, log as below. and in DTSI customer have change the limited from 105 to 125, but it still reset automatically. do you know why?
customer use below code to read the Temp.
while true
do
ret=`cat /sys/devices/virtual/thermal/thermal_zone0/temp`
ret1=`cat /sys/devices/virtual/thermal/thermal_zone1/temp`
ret2=`cat /sys/devices/virtual/thermal/thermal_zone2/temp`
echo " thermal_zone0‘s temp = ${ret} thermal_zone1’s temp = ${ret1} thermal_zone2’s temp = ${ret2} " >> /dev/console
sleep 0.5
done

@€ @ € @ €@ € € @@@€ €@€ € €@ € @@@ € €@€@@ @ @€ € @@ @€€ @@ @@€ @@€@ @@@
@@@€ € € @ @@ @ € @€€ € @ €@@@@ € @ € @ @@@@@@ @@ @ @@€ ! € @ @ @€( €€ €(@ @@@(
@ @ @@@@ @ @ @ @@@€ @@@€ @ ( (@€ @@(@(@(
( @ €! !
( ! (@ @H@( @( @ ((@ @€(@@ @@@€ P H @(P @ ( @è(
U-Boot SPL 2021.01-gfed177f5 (Dec 20 2023 - 03:33:38 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
am62a_init: board_init_f done
am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0
Trying to boot from MMC1
add by yong, spl_mmc_boot_mode, boot_device=9 devstat:0x4b, bootmode_cfg:0x0
add by yong, boot_mode=3
am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0
Authentication passed
am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0
Authentication passed
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0
am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0
init_env from device 9 not supported!
Starting ATF on ARM64 core...
NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
NOTICE: BL31: Built : 11:09:43, Feb 27 2023
U-Boot SPL 2021.01-gfed177f5 (Dec 20 2023 - 03:36:52 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
am62a_init: board_init_f done
am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0
Trying to boot from MMC1
add by yong, spl_mmc_boot_mode, boot_device=9 devstat:0x4b, bootmode_cfg:0x0
add by yong, boot_mode=3
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
U-Boot 2021.01-gfed177f5 (Dec 20 2023 - 03:36:52 +0800), Build: jenkins-DFMC_S73-Pipe_DFMC_S73-AM62A_OS-132
SoC: AM62AX SR1.0 HS-FS
Model: Texas Instruments AM62A7 SK
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed 1
DRAM: 1 GiB
MMC: mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed 1
Press 'ctrl+c' to stop autoboot: 2
MMC Device 2 not found
no mmc device at slot 2
SD/MMC found on device 2
19147264 bytes read in 110 ms (166 MiB/s)
35716 bytes read in 5 ms (6.8 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=PARTUUID=8d5e2621-747c-4dce-89bf-3ecab20ba9ad rw rootfstype=ext4 rootwait quiet
Loading Device Tree to 000000008fef4000, end 000000008fffffff ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.10.168-g921b2aae334b (uidq1391@hzh5302u) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #1 SMP PREEMPT Wed Dec 20 03:25:36 CST 2023
[ 0.000000] Machine model: Texas Instruments AM62A7 SK
[ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[ 0.000000] printk: bootconsole [ns16550a0] enabled
[ 0.000000] cma: Failed to reserve 512 MiB
[ 0.044486] omap-mailbox 29030000.mailbox: no available mbox devices found
[ 0.184772] pca953x 1-0023: failed writing register
[ 0.715461] pinctrl-single f4000.pinctrl: pin PIN80 already requested by 8000000.ethernet; cannot claim for 600000.gpio
[ 0.726260] pinctrl-single f4000.pinctrl: pin-80 (600000.gpio) status -22
[ 0.733043] pinctrl-single f4000.pinctrl: could not request pin 80 (PIN80) from group main-csi2-cam-pins-default on device pinctrl-single
[ 0.745455] davinci_gpio 600000.gpio: Error applying setting, reverse things back
[ 0.756592] pca953x 1-0022: failed writing register
[ 0.771168] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
[ 0.779145] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
[ 0.786521] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
[ 3.336091] vdec 30210000.video-codec: IRQ index 0 not found
[ 3.342685] vdec 30210000.video-codec: failed to get irq resource
[ 3.353344] ovx3c 2-0036: failed to read chip id 430358
[ 3.361654] k3_r5_rproc bus@f0000:bus@4000000:r5fss@79000000: SoC supports only single core R5 but num_cores is set to 0
[ 3.379612] platform 78000000.r5f: configured R5F for IPC-only mode
[ 3.386988] platform 78000000.r5f: R5F core initialized in IPC-only mode
[ 4.490640] hub 2-0:1.0: config failed, hub doesn't have any ports! (err -19)
[ 4.500791] hub 4-0:1.0: config failed, hub doesn't have any ports! (err -19)
██████╗ ███████╗███████╗ █████╗ ██╗ ██╗ ███████╗██╗ ██╗
██╔â•â•██╗██╔â•â•â•â•â•██╔â•â•â•â•â•██╔â•â•██╗╚██╗ ██╔╠██╔â•â•â•â•â•██║ ██║
██║ ██║█████╗ ███████╗███████║ ╚████╔╠███████╗██║ ██║
██║ ██║██╔â•â•╠╚â•â•â•â•██║██╔â•â•██║ ╚██╔╠╚â•â•â•â•██║╚██╗ ██╔â•
██████╔â•███████╗███████║██║ ██║ ██║ ███████║ ╚████╔â•
╚â•â•â•â•â•╠╚â•â•â•â•â•â•â•╚â•â•â•â•â•â•â•╚â•╠╚â•╠╚â•╠╚â•â•â•â•â•â•╠╚â•â•â•â•
Kernel 5.10.168-g921b2aae334b on an aarch64 at 00:00:03
am62axx-evm login:
am62axx-evm login: [usbupdate] Find Update Pkg...
[usbupdate] update package can not be found in USB path!!!
am62axx-evm login:
am62axx-evm login:
am62axx-evm login:
am62axx-evm login:
am62axx-evm login: root
root@am62axx-evm:~#
root@am62axx-evm:~#
root@am62axx-evm:~#
root@am62axx-evm:~#
root@am62axx-evm:~#
root@am62axx-evm:~# cd /dto
-sh: cd: /dto: No such file or directory
root@am62axx-evm:~# cd /storage/
root@am62axx-evm:/storage#
root@am62axx-evm:/storage#
root@am62axx-evm:/storage# ls
ap_data boot.img lost+found manifest.xml module.json other ppsshm.lock soc.zip svp_data test.sh update update_program.out vlan10_vsomeip.log
root@am62axx-evm:/storage# ./test.sh
thermal_zone0's temp=38046 thermal_zone1's temp=38983 thermal_zone2's temp=39450
thermal_zone0's temp=38046 thermal_zone1's temp=38515 thermal_zone2's temp=39683
thermal_zone0's temp=38749 thermal_zone1's temp=38749 thermal_zone2's temp=39683
thermal_zone0's temp=38983 thermal_zone1's temp=39216 thermal_zone2's temp=39683
thermal_zone0's temp=38749 thermal_zone1's temp=39216 thermal_zone2's temp=40148
thermal_zone0's temp=38515 thermal_zone1's temp=39216 thermal_zone2's temp=39450
thermal_zone0's temp=39216 thermal_zone1's temp=39216 thermal_zone2's temp=39216
thermal_zone0's temp=38515 thermal_zone1's temp=38515 thermal_zone2's temp=39216
thermal_zone0's temp=38046 thermal_zone1's temp=38515 thermal_zone2's temp=39216
thermal_zone0's temp=38046 thermal_zone1's temp=38280 thermal_zone2's temp=39216
thermal_zone0's temp=38280 thermal_zone1's temp=37811 thermal_zone2's temp=38983
thermal_zone0's temp=38280 thermal_zone1's temp=38046 thermal_zone2's temp=40148
thermal_zone0's temp=38280 thermal_zone1's temp=38046 thermal_zone2's temp=39916
thermal_zone0's temp=38046 thermal_zone1's temp=38280 thermal_zone2's temp=39216
thermal_zone0's temp=37576 thermal_zone1's temp=38515 thermal_zone2's temp=40148
thermal_zone0's temp=38515 thermal_zone1's temp=38983 thermal_zone2's temp=38983
thermal_zone0's temp=38046 thermal_zone1's temp=38046 thermal_zone2's temp=38983
thermal_zone0's temp=38749 thermal_zone1's temp=38280 thermal_zone2's temp=39916
thermal_zone0's temp=38749 thermal_zone1's temp=38280 thermal_zone2's temp=39683
thermal_zone0's temp=38983 thermal_zone1's temp=38983 thermal_zone2's temp=39916
thermal_zone0's temp=39450 thermal_zone1's temp=38983 thermal_zone2's temp=40845
thermal_zone0's temp=41540 thermal_zone1's temp=41771 thermal_zone2's temp=42922
thermal_zone0's temp=44297 thermal_zone1's temp=44297 thermal_zone2's temp=45209
thermal_zone0's temp=47472 thermal_zone1's temp=47021 thermal_zone2's temp=48819
thermal_zone0's temp=50602 thermal_zone1's temp=50602 thermal_zone2's temp=52591
thermal_zone0's temp=52811 thermal_zone1's temp=52811 thermal_zone2's temp=54781
thermal_zone0's temp=55216 thermal_zone1's temp=55216 thermal_zone2's temp=58024
thermal_zone0's temp=57810 thermal_zone1's temp=57379 thermal_zone2's temp=60160
thermal_zone0's temp=60584 thermal_zone1's temp=60372 thermal_zone2's temp=61431
thermal_zone0's temp=61642 thermal_zone1's temp=61853 thermal_zone2's temp=63114
thermal_zone0's temp=62905 thermal_zone1's temp=62695 thermal_zone2's temp=64576
thermal_zone0's temp=63114 thermal_zone1's temp=63324 thermal_zone2's temp=65615
thermal_zone0's temp=64368 thermal_zone1's temp=64368 thermal_zone2's temp=67060
thermal_zone0's temp=66648 thermal_zone1's temp=66648 thermal_zone2's temp=69513
thermal_zone0's temp=68290 thermal_zone1's temp=68699 thermal_zone2's temp=70528
thermal_zone0's temp=68699 thermal_zone1's temp=70123 thermal_zone2's temp=71939
thermal_zone0's temp=69513 thermal_zone1's temp=70325 thermal_zone2's temp=72340
thermal_zone0's temp=70325 thermal_zone1's temp=70730 thermal_zone2's temp=72941
thermal_zone0's temp=71738 thermal_zone1's temp=72941 thermal_zone2's temp=74535
thermal_zone0's temp=72741 thermal_zone1's temp=73939 thermal_zone2's temp=75524
thermal_zone0's temp=74931 thermal_zone1's temp=75524 thermal_zone2's temp=76706
thermal_zone0's temp=76313 thermal_zone1's temp=75919 thermal_zone2's temp=78075
thermal_zone0's temp=75327 thermal_zone1's temp=76706 thermal_zone2's temp=79242
thermal_zone0's temp=77880 thermal_zone1's temp=77489 thermal_zone2's temp=78659
thermal_zone0's temp=77685 thermal_zone1's temp=79242 thermal_zone2's temp=79823
thermal_zone0's temp=78075 thermal_zone1's temp=78854 thermal_zone2's temp=80787
thermal_zone0's temp=79629 thermal_zone1's temp=78659 thermal_zone2's temp=81363
thermal_zone0's temp=80787 thermal_zone1's temp=80979 thermal_zone2's temp=81938
thermal_zone0's temp=79823 thermal_zone1's temp=81171 thermal_zone2's temp=82892
thermal_zone0's temp=81938 thermal_zone1's temp=81363 thermal_zone2's temp=83463
thermal_zone0's temp=82511 thermal_zone1's temp=83652 thermal_zone2's temp=83842
thermal_zone0's temp=84221 thermal_zone1's temp=84787 thermal_zone2's temp=85916
thermal_zone0's temp=84787 thermal_zone1's temp=85352 thermal_zone2's temp=87037
thermal_zone0's temp=84031 thermal_zone1's temp=84976 thermal_zone2's temp=87224
thermal_zone0's temp=84976 thermal_zone1's temp=85540 thermal_zone2's temp=88338
thermal_zone0's temp=85352 thermal_zone1's temp=86103 thermal_zone2's temp=88893
thermal_zone0's temp=86290 thermal_zone1's temp=87968 thermal_zone2's temp=89815
thermal_zone0's temp=85916 thermal_zone1's temp=87410 thermal_zone2's temp=90182
thermal_zone0's temp=87224 thermal_zone1's temp=88893 thermal_zone2's temp=90915
thermal_zone0's temp=88708 thermal_zone1's temp=89078 thermal_zone2's temp=91280
thermal_zone0's temp=89998 thermal_zone1's temp=90732 thermal_zone2's temp=92008
thermal_zone0's temp=90915 thermal_zone1's temp=90915 thermal_zone2's temp=93277
thermal_zone0's temp=92734 thermal_zone1's temp=92190 thermal_zone2's temp=94178
thermal_zone0's temp=92372 thermal_zone1's temp=93096 thermal_zone2's temp=93998
thermal_zone0's temp=93277 thermal_zone1's temp=94357 thermal_zone2's temp=95253
thermal_zone0's temp=94178 thermal_zone1's temp=94537 thermal_zone2's temp=95967
thermal_zone0's temp=94716 thermal_zone1's temp=95075 thermal_zone2's temp=96856
thermal_zone0's temp=94716 thermal_zone1's temp=95253 thermal_zone2's temp=97740
thermal_zone0's temp=95253 thermal_zone1's temp=96501 thermal_zone2's temp=97564
thermal_zone0's temp=96145 thermal_zone1's temp=96856 thermal_zone2's temp=98445
thermal_zone0's temp=96501 thermal_zone1's temp=97033 thermal_zone2's temp=98972
thermal_zone0's temp=97210 thermal_zone1's temp=98093 thermal_zone2's temp=99147
thermal_zone0's temp=96856 thermal_zone1's temp=97740 thermal_zone2's temp=100369
thermal_zone0's temp=97564 thermal_zone1's temp=99147 thermal_zone2's temp=100717
thermal_zone0's temp=98445 thermal_zone1's temp=98796 thermal_zone2's temp=101064
thermal_zone0's temp=98972 thermal_zone1's temp=98972 thermal_zone2's temp=100891
thermal_zone0's temp=100021 thermal_zone1's temp=99846 thermal_zone2's temp=101757
thermal_zone0's temp=100369 thermal_zone1's temp=99497 thermal_zone2's temp=102619
thermal_zone0's temp=100891 thermal_zone1's temp=100717 thermal_zone2's temp=103134
thermal_zone0's temp=100891 thermal_zone1's temp=101930 thermal_zone2's temp=102963
thermal_zone0's temp=102102 thermal_zone1's temp=101930 thermal_zone2's temp=103819
thermal_zone0's temp=101238 thermal_zone1's temp=102102 thermal_zone2's temp=104502
thermal_zone0's temp=101930 thermal_zone1's temp=102275 thermal_zone2's temp=104502
thermal_zone0's temp=102619 thermal_zone1's temp=103134 thermal_zone2's temp=105012
thermal_zone0's temp=103819 thermal_zone1's temp=104161 thermal_zone2's temp=105012
thermal_zone0's temp=104161 thermal_zone1's temp=103819 thermal_zone2's temp=105182
thermal_zone0's temp=104161 thermal_zone1's temp=104161 thermal_zone2's temp=104842
thermal_zone0's temp=104842 thermal_zone1's temp=104161 thermal_zone2's temp=105521
thermal_zone0's temp=104842 thermal_zone1's temp=104161 thermal_zone2's temp=105860
thermal_zone0's temp=105521 thermal_zone1's temp=104842 thermal_zone2's temp=106029
thermal_zone0's temp=105352 thermal_zone1's temp=105860 thermal_zone2's temp=106366
thermal_zone0's temp=104842 thermal_zone1's temp=104672 thermal_zone2's temp=105182
thermal_zone0's temp=103990 thermal_zone1's temp=104331 thermal_zone2's temp=104331
thermal_zone0's temp=105012 thermal_zone1's temp=104842 thermal_zone2's temp=104502
thermal_zone0's temp=104842 thermal_zone1's temp=105521 thermal_zone2's temp=104502
thermal_zone0's temp=105521 thermal_zone1's temp=105860 thermal_zone2's temp=106029
thermal_zone0's temp=105860 thermal_zone1's temp=106197 thermal_zone2's temp=107543
thermal_zone0's temp=107208 thermal_zone1's temp=108045 thermal_zone2's temp=109045
thermal_zone0's temp=107711 thermal_zone1's temp=108546 thermal_zone2's temp=109212
thermal_zone0's temp=108045 thermal_zone1's temp=109212 thermal_zone2's temp=109875
thermal_zone0's temp=108546 thermal_zone1's temp=109709 thermal_zone2's temp=110371
thermal_zone0's temp=108713 thermal_zone1's temp=109875 thermal_zone2's temp=111194
thermal_zone0's temp=109544 thermal_zone1's temp=110701 thermal_zone2's temp=111523
thermal_zone0's temp=109378 thermal_zone1's temp=110536 thermal_zone2's temp=112341
thermal_zone0's temp=110206 thermal_zone1's temp=111194 thermal_zone2's temp=112505
thermal_zone0's temp=110206 thermal_zone1's temp=111523 thermal_zone2's temp=112341
thermal_zone0's temp=110701 thermal_zone1's temp=111359 thermal_zone2's temp=112994
thermal_zone0's temp=110865 thermal_zone1's temp=111687 thermal_zone2's temp=112831
thermal_zone0's temp=111523 thermal_zone1's temp=112178 thermal_zone2's temp=113319
thermal_zone0's temp=112014 thermal_zone1's temp=112668 thermal_zone2's temp=112831
thermal_zone0's temp=110865 thermal_zone1's temp=112341 thermal_zone2's temp=113806
thermal_zone0's temp=111030 thermal_zone1's temp=111687 thermal_zone2's temp=113481
thermal_zone0's temp=111359 thermal_zone1's temp=111523 thermal_zone2's temp=113806
thermal_zone0's temp=111687 thermal_zone1's temp=111687 thermal_zone2's temp=114291
thermal_zone0's temp=111030 thermal_zone1's temp=110865 thermal_zone2's temp=113644
thermal_zone0's temp=110536 thermal_zone1's temp=110865 thermal_zone2's temp=113481
thermal_zone0's temp=111194 thermal_zone1's temp=110536 thermal_zone2's temp=113319
thermal_zone0's temp=111523 thermal_zone1's temp=110865 thermal_zone2's temp=114130
thermal_zone0's temp=111523 thermal_zone1's temp=111194 thermal_zone2's temp=114453
thermal_zone0's temp=112014 thermal_zone1's temp=111523 thermal_zone2's temp=114453
thermal_zone0's temp=111851 thermal_zone1's temp=111687 thermal_zone2's temp=114453
thermal_zone0's temp=112668 thermal_zone1's temp=111851 thermal_zone2's temp=115098
thermal_zone0's temp=113156 thermal_zone1's temp=112668 thermal_zone2's temp=115580
thermal_zone0's temp=113644 thermal_zone1's temp=113481 thermal_zone2's temp=116381
thermal_zone0's temp=114130 thermal_zone1's temp=114453 thermal_zone2's temp=116860
thermal_zone0's temp=113968 thermal_zone1's temp=114130 thermal_zone2's temp=117178
thermal_zone0's temp=114937 thermal_zone1's temp=115419 thermal_zone2's temp=116860
thermal_zone0's temp=114776 thermal_zone1's temp=114937 thermal_zone2's temp=117337
thermal_zone0's temp=114937 thermal_zone1's temp=115740 thermal_zone2's temp=118289
thermal_zone0's temp=116061 thermal_zone1's temp=116061 thermal_zone2's temp=118130
thermal_zone0's temp=116061 thermal_zone1's temp=116221 thermal_zone2's temp=117814
thermal_zone0's temp=116540 thermal_zone1's temp=117337 thermal_zone2's temp=118130
thermal_zone0's temp=116061 thermal_zone1's temp=116381 thermal_zone2's temp=118605
thermal_zone0's temp=116540 thermal_zone1's temp=116540 thermal_zone2's temp=119235
thermal_zone0's temp=117178 thermal_zone1's temp=116381 thermal_zone2's temp=119078
thermal_zone0's temp=117178 thermal_zone1's temp=117496 thermal_zone2's temp=119550
thermal_zone0's temp=117337 thermal_zone1's temp=117178 thermal_zone2's temp=119864
thermal_zone0's temp=116381 thermal_zone1's temp=116860 thermal_zone2's temp=120020
thermal_zone0's temp=116381 thermal_zone1's temp=116700 thermal_zone2's temp=119393
thermal_zone0's temp=117178 thermal_zone1's temp=117337 thermal_zone2's temp=120334
thermal_zone0's temp=116860 thermal_zone1's temp=116860 thermal_zone2's temp=120646
thermal_zone0's temp=117814 thermal_zone1's temp=117496 thermal_zone2's temp=120958
thermal_zone0's temp=117972 thermal_zone1's temp=118130 thermal_zone2's temp=120958
thermal_zone0's temp=117972 thermal_zone1's temp=118605 thermal_zone2's temp=121736
thermal_zone0's temp=118605 thermal_zone1's temp=118763 thermal_zone2's temp=121581
thermal_zone0's temp=118763 thermal_zone1's temp=118920 thermal_zone2's temp=121891
thermal_zone0's temp=119078 thermal_zone1's temp=120020 thermal_zone2's temp=122356
thermal_zone0's temp=119393 thermal_zone1's temp=120646 thermal_zone2's temp=121270
thermal_zone0's temp=119235 thermal_zone1's temp=120177 thermal_zone2's temp=122201
thermal_zone0's temp=120490 thermal_zone1's temp=120802 thermal_zone2's temp=122511
U-Boot SPL 2021.01-gfed177f5 (Dec 20 2023 - 03:33:38 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
am62a_init: board_init_f done
am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0
Trying to boot from MMC1
add by yong, spl_mmc_boot_mode, boot_device=9 devstat:0x4b, bootmode_cfg:0x0
add by yong, boot_mode=3
am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0
Authentication passed
am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0
Authentication passed
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0
am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0
init_env from device 9 not supported!
Starting ATF on ARM64 core...
NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
NOTICE: BL31: Built : 11:09:43, Feb 27 2023
U-Boot SPL 2021.01-gfed177f5 (Dec 20 2023 - 03:36:52 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
am62a_init: board_init_f done
am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0
Trying to boot from MMC1
add by yong, spl_mmc_boot_mode, boot_device=9 devstat:0x4b, bootmode_cfg:0x0
add by yong, boot_mode=3
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
U-Boot 2021.01-gfed177f5 (Dec 20 2023 - 03:36:52 +0800), Build: jenkins-DFMC_S73-Pipe_DFMC_S73-AM62A_OS-132
SoC: AM62AX SR1.0 HS-FS
Model: Texas Instruments AM62A7 SK
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed 1
DRAM: 1 GiB
MMC: mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed 1
Press 'ctrl+c' to stop autoboot: 2
MMC Device 2 not found
no mmc device at slot 2
SD/MMC found on device 2
19147264 bytes read in 110 ms (166 MiB/s)
35716 bytes read in 4 ms (8.5 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=PARTUUID=8d5e2621-747c-4dce-89bf-3ecab20ba9ad rw rootfstype=ext4 rootwait quiet
Loading Device Tree to 000000008fef4000, end 000000008fffffff ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.10.168-g921b2aae334b (uidq1391@hzh5302u) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #1 SMP PREEMPT Wed Dec 20 03:25:36 CST 2023
[ 0.000000] Machine model: Texas Instruments AM62A7 SK
[ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[ 0.000000] printk: bootconsole [ns16550a0] enabled
[ 0.000000] cma: Failed to reserve 512 MiB
[ 0.044529] omap-mailbox 29030000.mailbox: no available mbox devices found
[ 0.184818] pca953x 1-0023: failed writing register
[ 0.715258] pinctrl-single f4000.pinctrl: pin PIN80 already requested by 8000000.ethernet; cannot claim for 600000.gpio
[ 0.726061] pinctrl-single f4000.pinctrl: pin-80 (600000.gpio) status -22
[ 0.732844] pinctrl-single f4000.pinctrl: could not request pin 80 (PIN80) from group main-csi2-cam-pins-default on device pinctrl-single
[ 0.745255] davinci_gpio 600000.gpio: Error applying setting, reverse things back
[ 0.756421] pca953x 1-0022: failed writing register
[ 0.770779] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
[ 0.778750] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
[ 0.786184] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
[ 3.341355] ovx3c 2-0036: failed to read chip id 430358
[ 3.350175] vdec 30210000.video-codec: IRQ index 0 not found
[ 3.358599] vdec 30210000.video-codec: failed to get irq resource
[ 3.378102] k3_r5_rproc bus@f0000:bus@4000000:r5fss@79000000: SoC supports only single core R5 but num_cores is set to 0
[ 3.413362] platform 78000000.r5f: configured R5F for IPC-only mode
[ 3.420675] platform 78000000.r5f: R5F core initialized in IPC-only mode
[ 4.516169] hub 2-0:1.0: config failed, hub doesn't have any ports! (err -19)
[ 4.526466] hub 4-0:1.0: config failed, hub doesn't have any ports! (err -19)
██████╗ ███████╗███████╗ █████╗ ██╗ ██╗ ███████╗██╗ ██╗
██╔â•â•██╗██╔â•â•â•â•â•██╔â•â•â•â•â•██╔â•â•██╗╚██╗ ██╔╠██╔â•â•â•â•â•██║ ██║
██║ ██║█████╗ ███████╗███████║ ╚████╔╠███████╗██║ ██║
██║ ██║██╔â•â•╠╚â•â•â•â•██║██╔â•â•██║ ╚██╔╠╚â•â•â•â•██║╚██╗ ██╔â•
██████╔â•███████╗███████║██║ ██║ ██║ ███████║ ╚████╔â•
╚â•â•â•â•â•╠╚â•â•â•â•â•â•â•╚â•â•â•â•â•â•â•╚â•╠╚â•╠╚â•╠╚â•â•â•â•â•â•╠╚â•â•â•â•
Kernel 5.10.168-g921b2aae334b on an aarch64 at 00:01:49
am62axx-evm login: [usbupdate] Find Update Pkg...
[usbupdate] update package can not be found in USB path!!!
BR,
Biao