This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VE-Q1: DCC3.1 Error in capturing the RAW image

Part Number: TDA4VE-Q1

Hello,

We use imx219 and DCC3.1 for ISP tuning.

Currently: imx219 can capture images normally; the development board and DCC IP are configured correctly; the DCC software can process offline images and run normally.

But when we used imx219 to save RAW images in real time, the following error occurred. Solve.

Request to get RAW image from Target : 192.168.1.30

Loaded communication DLL:itCommun.dll

Error in capturing the RAW image

Request to get YUV image from Target : 192.168.1.30

Loaded communication DLL:itCommun.dll

Error in capturing the YUV image

Regards,

Gary