We used AM6422 customized board, and we want to enable the MCU RTI_WDT in R5 SPL. When it block in R5 SPL, the MCU RTI_WDT can reset the system.
What I did now is as below,
Dts,
In k3-am64-mcu.dtsi
mcu_rti1: rti@40610000 {
compatible = "ti,j7-rti-wdt";
reg = <0x0 0x40610000 0x0 0x100>;
clocks = <&k3_clks 135 0>;
power-domains = <&k3_pds 135 TI_SCI_PD_SHARED>;
assigned-clocks = <&k3_clks 135 0>;
assigned-clock-parents = <&k3_clks 135 4>;
};
R5 config,
Resetting on cold boot to workaround ErrataID:i2331
resetting ...
U-Boot SPL 2021.01-g7653b040e1 (Jan 18 2024 - 10:31:13 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0016 '22.1.1--v2022.01 (Terrific Llam')
SPL initial stack usage: 13376 bytes
WDT: Not found!
Trying to boot from SPI
Starting ATF on ARM64 core...