This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need help in Part Number Selection

Dear Support,

I need help in selecting a Processor with below interfaces only. Suggest a optimal one. Anything more than these interface is no requirement. Mostly bare metal software will be used. Need option for Linux/RTOS too.

1. 2 SPI interfaces running at maximum 50MHz

2. eMMC for NAND Flash with 32GB support

3. USB 2.0 for data storing

Regards,

Erfan

  • Hello Erfan,

    I recommend considering the STM32 series microcontroller particularly models like the STM32F4 or STM32H7. They offer the necessary interfaces. 2 SPI interfaces running at up to 50MHz, MMC support for NAND Flash up to 32GB, and USB 2.0 for data storage. These microcontrollers are well-suited for bare metal software and support both Linux and RTOS environments.

    Hope this helps!