This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am referring the collaterals for the below EVM / SK.
SK-AM64B (PROC100A), TMDS64EVM (PROC101C)
Is there any Update to be Done on the collaterals to reuse in my custom design.
Hi Board designers,
Here are some recommended updates based on the learnings for performance improvements.
Schematics - Design Value Updates
1. VCC_3V3_SYS LOAD SWITCH
SoC IO supply rails have slew rate requirements specified.
Refer Power Supply Slew Rate Requirement section of the data sheet.
Add a cap 220 pF or higher on the Load switch CT (Switch slew rate control) pin.
2. SD card power reset Load switch
Add a cap 220 pF or higher on the Load switch CT (Switch slew rate control) pin.
3. eMMC supply decap
Add decaps as required to the eMMC memory supply rails
4. USB VBUS divider
5. Provision to Bypass CMC
6. USB power switch
Use power switch with OC indication. Connect the OC output of the power switch to SoC input
7. SoC clock MCU_OSC0_XI. MCU_OSC0_XO - connecting external clock
DNI the R and C placed at the output of the clock buffer connected to the MCU OSC0 clock input. Placement of these components reduces the amplitude and could affect the performance
8. SoC MCU_OSC0_XO termination - when using external clock
Data sheet section reference : MCU_OSC0 LVCMOS Digital Clock Source
Do not leave XO un connected
The oscillator was designed to measure the differential voltage between XI and XO, for creating a internal reference clock. So there is no guarantee they will get the correct differential input voltage if the XO pin is allowed to float. The datasheet clearly shows this pin needs to be connected to VSS when using an LVCMOS clock source.
9. Ethernet PHY updates
10. Caution with EPHY 1V and VPP 1.8V LDO
Miniature DQN package used.
Package Outline
PCB pads
There is a likely chance of assembly error due to the LOD outline, pins orientation and the land pattern (pads and pitch)
Take note of the following
EPHY 1.8V supply pins when not used should not be shorted
Note the recommended caps for the EPHY supplies
Note the Rbias R and C values
Note the pulldown for the EPHY Reset
11 EXTINTn RC and pullup
EXTINTn is a open drain output type IO buffer. The IO has slew rate limit requirements when pulled to 3.3V/
Add an RC to limit the slew rate.
Regards,
Sreenivasa
Hi Board designers,
Refer below workarounds when load switch is not used for resetting the SD card power supply and the supply is fixed to 3.3V
Given below are the list of various workarounds that can be done in the device tree node to get SD card working. The workarounds are ordered in increasing order of reducing performance.
All the changes mentioned below, are to be done in the MMCSD device tree node corresponding to the SD instance. This is usually the first (index starting from zero) instance.
· &sdhci1 {· /* SD/MMC */· vmmc-supply = <&vdd_mmc1>;· vqmmc-supply = <&vdd_sd_dv>;· pinctrl-names = "default";· pinctrl-0 = <&main_mmc1_pins_default>;· ti,driver-strength-ohm = <50>;· disable-wp;· sdhci-caps-mask = <0x00000006 0x00000000>; /* Limiting to SDR50 speed mode */· };
· &sdhci1 {· /* SD/MMC */· vmmc-supply = <&vdd_mmc1>;· vqmmc-supply = <&vdd_sd_dv>;· pinctrl-names = "default";· pinctrl-0 = <&main_mmc1_pins_default>;· ti,driver-strength-ohm = <50>;· disable-wp;· no-1-8-v; /* disabling all the UHS modes */};
Regards,
Sreenivasa
Hi Board designers,
MMC0 PCB Connectivity Requirements
we have issues with an eMMC connected to MMC0 of a AM6254 processor on a custom board.
In the datasheet of the AM625 processors we found layout requirements for the MMC0 interface.
Does this "min" specification mean that the traces of the MMC0 interfaces MUST have a minimum length? If yes can you specify this in inches or mm?
Yes, there is a minimum trace delay requirement for this peripheral.
The delay values are defined with the unit of picoseconds (ps). You will need to determine the propagation velocity of each signal trace on your specific PCB design to know how much additional trace needs to be inserted to achieve the appropriate delay.
Regards,
Sreenivasa
Hi Board designers,
To implement UHS-I refer below steps:
The SD card interface pullups have to be connected to the 3.3V_1.8V VDDSHV_SDIO switched supply output from the PMIC
The SD card needs to be powered using a fixed 3.3V supply.
The 3.3V supply to the SD card needs to be switched through a power switch
Provision to reset the power switch using SOC IOs is recommended
An ANDing logic is recommend to reset the SD cars power switch.
The SOC VDDSHV5 supply needs to be connected to the .3V_1.8V VDDSHV_SDIO switched supply output from the PMIC
Regards,
Sreenivasa
Hi Board designers,
refer below FAQ for queries related to MCU_OSC0 Start-up Time
Regards,
Sreenivasa