This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: CUSTOM BOARD, AM243x and AM64x: enet_lwip_cpsw example: Loader:Verification failed - DDR RAM usage not given?

Part Number: AM6442
Other Parts Discussed in Thread: SYSCONFIG

Hello everyone,

getting following error when trying to load the example enet_lwip_cpsw_am64x:

I already tried building loading the sbl_null before example, where I initialize the DDR RAM. I tried removing "System Deiinit" from the sbl_null main src but it also didn't work.

Does someone have an advice?

Thank you very much.

  • Hello again,

    I only want to update and give more informations about this: 

    My custom Board has a LPDDR4 RAM with 1GB. I tested it already writting and reading. I also  generated files with the sysconfig DDR tool and replaced the according files with new ones. 

    I'm still getting the message: Verification Failed: address 0x80....

    Still no clue why...

  • Hello again,

    I won't give up untill I found an answer to this.

    And I really hope that someone can give me an advice, because as it seems, nothing works when trying debugging on the external DDR-RAM.

    I tried loading the hello world example into the DDR-RAM. It seems that it won't also work, so my question, why?

    I use the "load_dsmc_hsfs" script along with a modified version of the AM243x_GP_EVM script. 

    /* Copyright (c) 2021, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */
    
    #define DDR4 1
    #define LPDDR4 2
    #define MHZ25 1
    int DDR_MODE; // set in DDR GEL functions based on board
    unsigned int AM24_DDRSS_SS_BASE;
    unsigned int AM24_DDRSS_CTL_BASE;
    
    memorymap_init() {
      GEL_MapAddStr(0x00000000, 0, 0x00008000, "R|W|RAM",
                    0); // R5TCMA, SRAM
      GEL_MapAddStr(0x41010000, 0, 0x00008000, "R|W|RAM",
                    0); // R5TCMB0, SRAM
      GEL_MapAddStr(0x70060000, 0, 0x00008000, "R|W|RAM",
                    0); // MCU NON CACHEABLE
      GEL_MapAddStr(0x70080000, 0, 0x140000, "R|W|RAM",
                    0); // MSRAM
      GEL_MapAddStr(0x80000000, 0, 0x40000000, "R|W|RAM",
                    0); // 1G DDR4 external memory
    }
    
    StartUp() {
      GEL_LoadGel("$(GEL_file_dir)/../AM24_common/AM24_common.gel");
      // Load own Configs..
      GEL_LoadGel("$(GEL_file_dir)/AM243x-DDRConfig.gel");
    
      // GEL_LoadGel("$(GEL_file_dir)/AM24x-DDR4-1600MTs.gel");
    
      GEL_LoadGel("$(GEL_file_dir)/AM24_DDRSS_addr_map_sfr_offs_ew_16bit.gel");
      GEL_LoadGel("$(GEL_file_dir)/AM24_DDRSS_Config.gel");
      GEL_LoadGel("$(GEL_file_dir)/AM24_DDRSS_RegDump.gel");
      GEL_LoadGel("$(GEL_file_dir)/AddrMapCheck.gel");
      GEL_LoadGel("$(GEL_file_dir)/../AM24_PLL/AM24_PLL_MMR.gel");
      GEL_LoadGel("$(GEL_file_dir)/../AM24_PLL/AM24_PLL.gel");
      GEL_LoadGel("$(GEL_file_dir)/../AM24_PLL/AM24_PLL_DDR_configurations.gel");
    
      /*------------------ Memory Map Config -------------------*/
      GEL_MapOff();
      GEL_MapReset();
      memorymap_init();
      GEL_MapOn();
    
      DDR_MODE = LPDDR4;
    }
    
    OnTargetConnect() { DDR_Init(); }
    

    The own configs are made through the syscfg-ddr tool. I also changed the default board_regInit.h file with the recent DDR4-adaptation. Still I can't load a program into the DDR4 or only parts of a program, although the DDR seems to be initialized.

    Does someone know what I am doing wrong?

    Thank you.

  • Issac, i'm not sure what is going on .  You said earlier that you have tested the DDR and you can read and write to it.  Can you give more details on this test?  When you get the error, can you open a Memory Browser window and write/read that location? 

    Another issue is that you load a DDR4 configuration at line 56, but you are setting DDR_MODE to LPDDR4 on line 72.  Are you using an AM64x or AM243x?

    Regards,

    James

  • Hello @JDD,

    I can, if I run code writting to address 0x8000000 up to 1 GB length, I'm able to read and write. Still, if I try to debug code per CCS, loading it via JTAG into RAM, the error mentioned here appears.

    I thought that this is issued by the address map as the default GEL file doesn't seem to load the addressspaces, so I edited it:

    diff --git a/ccs/ccs_base/emulation/gel/AM24x/AM24_DDRSS/AM24x_GP_EVM.gel b/ccs/ccs_base/emulation/gel/AM24x/AM24_DDRSS/AM24x_GP_EVM.gel
    index bb42558..4bc1e8f 100644
    --- a/ccs/ccs_base/emulation/gel/AM24x/AM24_DDRSS/AM24x_GP_EVM.gel
    +++ b/ccs/ccs_base/emulation/gel/AM24x/AM24_DDRSS/AM24x_GP_EVM.gel
    @@ -28,27 +28,48 @@
      * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
      * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */
     
    -#define DDR4 	 1
    -#define LPDDR4 	 2
    -#define MHZ25    1
    -int DDR_MODE;	//set in DDR GEL functions based on board
    -unsigned int AM24_DDRSS_SS_BASE;	
    +#define DDR4 1
    +#define LPDDR4 2
    +#define MHZ25 1
    +int DDR_MODE; // set in DDR GEL functions based on board
    +unsigned int AM24_DDRSS_SS_BASE;
     unsigned int AM24_DDRSS_CTL_BASE;
     
    -StartUp(){
    -	GEL_LoadGel("$(GEL_file_dir)/../AM24_common/AM24_common.gel");
    -	GEL_LoadGel("$(GEL_file_dir)/AM24x-DDR4-1600MTs.gel");
    -	GEL_LoadGel("$(GEL_file_dir)/AM24_DDRSS_addr_map_sfr_offs_ew_16bit.gel");
    -    GEL_LoadGel("$(GEL_file_dir)/AM24_DDRSS_Config.gel");
    -	GEL_LoadGel("$(GEL_file_dir)/AM24_DDRSS_RegDump.gel");
    -	GEL_LoadGel("$(GEL_file_dir)/AddrMapCheck.gel");
    -	GEL_LoadGel("$(GEL_file_dir)/../AM24_PLL/AM24_PLL_MMR.gel");
    -	GEL_LoadGel("$(GEL_file_dir)/../AM24_PLL/AM24_PLL.gel");
    -	GEL_LoadGel("$(GEL_file_dir)/../AM24_PLL/AM24_PLL_DDR_configurations.gel");
    -	
    -	DDR_MODE = DDR4;
    -}	
    -
    -OnTargetConnect(){
    -	//DDR_Init();
    +memorymap_init() {
    +  GEL_MapAddStr(0x00000000, 0, 0x00008000, "R|W|RAM",
    +                0); // R5TCMA, SRAM
    +  GEL_MapAddStr(0x41010000, 0, 0x00008000, "R|W|RAM",
    +                0); // R5TCMB0, SRAM
    +  GEL_MapAddStr(0x70060000, 0, 0x00008000, "R|W|RAM",
    +                0); // MCU NON CACHEABLE
    +  GEL_MapAddStr(0x70080000, 0, 0x140000, "R|W|RAM",
    +                0); // MSRAM
    +  GEL_MapAddStr(0x80000000, 0, 0x40000000, "R|W|RAM",
    +                0); // 1G DDR4 external memory
     }
    +
    +StartUp() {
    +  GEL_LoadGel("$(GEL_file_dir)/../AM24_common/AM24_common.gel");
    +  // Load own Configs..
    +  GEL_LoadGel("$(GEL_file_dir)/AM243x-DDRConfig.gel");
    +
    +  // GEL_LoadGel("$(GEL_file_dir)/AM24x-DDR4-1600MTs.gel");
    +
    +  GEL_LoadGel("$(GEL_file_dir)/AM24_DDRSS_addr_map_sfr_offs_ew_16bit.gel");
    +  GEL_LoadGel("$(GEL_file_dir)/AM24_DDRSS_Config.gel");
    +  GEL_LoadGel("$(GEL_file_dir)/AM24_DDRSS_RegDump.gel");
    +  GEL_LoadGel("$(GEL_file_dir)/AddrMapCheck.gel");
    +  GEL_LoadGel("$(GEL_file_dir)/../AM24_PLL/AM24_PLL_MMR.gel");
    +  GEL_LoadGel("$(GEL_file_dir)/../AM24_PLL/AM24_PLL.gel");
    +  GEL_LoadGel("$(GEL_file_dir)/../AM24_PLL/AM24_PLL_DDR_configurations.gel");
    +
    +  /*------------------ Memory Map Config -------------------*/
    +  GEL_MapOff();
    +  GEL_MapReset();
    +  memorymap_init();
    +  GEL_MapOn();
    +
    +  DDR_MODE = LPDDR4;
    +}
    +
    +OnTargetConnect() { DDR_Init(); }
    

    I'm currently using the AM23x HSFS ALV chip, but I also have a board with the AM64x, and I would like to get this working on both.

    PS.: Both boards use LPDDR

    Thank you very much! 

  • And Yes I can open while using an application without the DDR-RAM linked the addresses. Only the if I try loading an application via debugger it doesn't work. Here the basic Read/Write test:

  • And by that I mean that if I run the script only, the DDR-RAm seems not to be initialized.. although I already built a new target sciclient_ccs_init with the DDR-Ram initialization...