This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-J784S4: Instance for BIST

Part Number: PROCESSOR-SDK-J784S4


Hi TI Expert,

I am doing an example for BIST. I would like to use MCU1_0 to trigger the BIST for MCU1_1 and A72. I found the files SDK 08_06_00_14\sdl\src\sdl\lbist\soc\j784s4\sdl_lbist.h and SDK 08_06_00_14\sdl\src\sdl\pbist\soc\j784s4\sdl_pbist.h shows the definition of different core instances.

  • LBIST

Which core does "SDL_LBIST_HWPOST_INST_MCU" define? Is it only for MCU1_0 in MCU domain? Does it include MCU1_0 and MCU1_1 in MCU Domain? Is "SDL_LBIST_HWPOST_INST_SMS" WKUP_SMS in MCU domain?
Which cores does the red cycle define?
Which cores does the red cycle define?
  • PBIST

Which core does "SDL_PBIST_HWPOST_INST_MCU" define? Is it only for MCU1_0 in MCU domain? Does it include MCU1_0 and MCU1_1 in MCU Domain?

Which cores does the red cycle define?

Which cores does the red cycle define?

Which cores does the red cycle define?

Thanks

Dengkuan