Part Number: AM625
Hello,
Our product base on A625 SK EVM board will be flash by netboot, so our boot mode will be configured as followed:
| B0 | B1 | B2 | B3 | B4 | B5 | B6 | B7 | B8 | B9 | B10 | B11 | B12 | B13 | B14 | B15 |
| PLL Config | Primary Boot Mode | Primary Boot Mode Config | Backup Boot Mode | Backup Boot Mode Config | Reserved | ||||||||||
| 1 | 1 | 0 | 1 | 0 | 0 | 1 | 1 | 0 | 1 | 0 | 0 | 1 | 0 | 0 | 0 |
So we set primary boot to eMMC and backup on Ethernert RGMII1.
Here are my questions :
- Could you confirm that this configuration is correct ?
- During the production cycle when the board with an empty eMMC will boot can we be sure that the backup bootmode will be used ?
- What are the condition that make the bootmode switch to backup mode ?
- When the eMMC is has been flashed, is there any when to disable the backup bootmode from ethernet ?
Thanks,
Regards,
Alexis.