I have tried the HUA demo on the Shannon and have not got the web interface to work.
I have installed ccs v5.03 that came with the EVM and also installed the MCSDK and got basic JTAG connectivity with the board working, i.e loading, running code etc.
My output was as follows in the CCS v5 console window.
I am using a Rev 1.0 version of the TMDXevm6678LE board.
I have an Ethernet cable connection between the board and my PC.
A usb connection between the board (560 emulation) and my PC.
I have the shunts positioned to use the USB as opposed to the RS 232 which I have also tried incidentally without success.
The other switch settings are
SW3 1-off,2-off,3-on,4-off
SW4 1-on,2-on,3-on,4-on
SW5 1-on,2-on,3-on,4-off
SW6 1-on,2-on,3-on,4-on
SW9 1-on,2-on
[C66xx_0] Start BIOS 6
[C66xx_0] HPDSPUA version 2.00.00.02 Beta 2
[C66xx_0] Setting hostname to TMDSEVMC6678L5356
[C66xx_0] Configuring DHCP client
[C66xx_0] QMSS successfully initialized
[C66xx_0] CPPI successfully initialized
[C66xx_0] PASS successfully initialized
[C66xx_0] Ethernet subsystem successfully initialized
[C66xx_0] eventId : 48 and vectId : 7
[C66xx_0] Verify_Init: Expected 16 entry count for gTxFreeQHnd queue 736, found 30 entries
[C66xx_0] Verify_Init: Expected 0 entry count for gRxQHnd= 704, found 11 entries
[C66xx_0] Verify_Init: Expected 0 entry count for Queue number = 0, found 1 entries
[C66xx_0] Verify_Init: Expected 0 entry count for Queue number = 704, found 11 entries
[C66xx_0] Verify_Init: Expected 0 entry count for Queue number = 4095, found 1 entries
[C66xx_0] Verify_Init: Expected 0 entry count for Queue number = 8192, found 1 entries
[C66xx_0] Warning:Queue handler Verification failed
[C66xx_0] Registration of the EMAC Successful, waiting for link up ..
[C66xx_0] Service Status: DHCPC : Enabled : : 000
[C66xx_0] Service Status: THTTP : Enabled : : 000
[C66xx_0] Service Status: DHCPC : Enabled : Running : 000
[C66xx_0] Service Status: DHCPC : Enabled : Fault : 002
I have also tried with SW9 set to 1-off, 2-off (i.e. using Static IP) and get an EMAC error.
Any assistance will be appreciated.
Thanks, Aamir