Part Number: AM623
Hi
We are having trouble achieving the input slew rates of 2.64V/ns ... 5V/ns for the RGMII signals defined in the AM62x Rev B datasheet (SPRSP58B), Table 7-33.
Are the values correct for 1.8V? Because the RMII interface, which uses the same pins, differentiates between 1.8V and 3.3V...
I also have another question for my better understanding. Is the input slew rate calculated from 10%/90% or 20%/80%?
Thank you very much and best regards
Marcel Kaltschmied