Hi,
Setup
- TDA4VE SOM on EVM boards
- Default Linux + RTOS images from SDK 9.1
- Software uses VPAC, OpenglES, R5F display node, TIDL
- Tivx modification - Default stride set to 64 e2e.ti.com/.../tda4vm-opengl-render-issue-when-migrating-from-sdk-08-02-xx-xx-to-sdk-08-05-xx-xx
Question
We are currently facing display corruption when using the R5F display node. We use a custom opengl node based on the mosaic one from visionapps and we pass a vximage directly to the display node.
The graph is called in an a vxProcessGraph() and our graph looks like:
inputs -> [opengl openvx node on A72] -> [display node on R5F] -> display port
The problem is that at random time (~1/400) we can see corruption in the Y and X axis
Here a non corrupted image as reference.
Is it a behavior that TI's observed in certain cases or a known issue in the SDK9.1 ?
Thanks,