This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62-SIP: AM62-SIP supplied

Part Number: SK-AM62-SIP

Hi TI!!!

I want to do a simpler design than the SK-AM62-SIP and I have the following questions?

I see that VDDSHV_SDIO (MCU side) it is powered through a regulator that is configured for 3.3V or 1.8V. However, the SD is powered with 3.3V.
Is it possible to supply VDDSHV_SDIO directly with VCC_3V3_SYS?

Can I keep VPP pulled down through a resistor?
Assuming that VPP has a pull down, in case I want to blow the fuse: Can I have a jumper to VCC_1V8 that allows me to put 1.8V on VPP?

When will the AM62-SIP be commercially available?

Thanks very much. Best Regards.