This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SOC:TDA4VH
version:8.60
quesion1:
OX05B1S output raw10.The captured RAW image is OK,After VPAC, the upper part of the horizontal stripe and the lower part of the screen appeared.
See the error image below.
raw and yuv in the attachment.
Whether VPAC supports data access in RAW10 format.
quesion2:
SOC:TDA4VH
version:8.60
SC233AT output RAW8,.The captured RAW image is OK.but When RAW images are entered into VPAC, VPAC crashes.
Whether VPAC supports data access in RAW8 format.
Hi quan,
I have repeated your problem on my side:
Could you provide knee points and black level? And what is the color pattern?
Regards,
Adam
HI:adam
I have solved this problem.
Refer to the SDK in IMX219, linear 10bit XML file,when i disable LSC ,the YUV is OK.
but i do not reson,Is the bit width of the data input to the LSC module incorrect?
HI:adam
..\imaging\sensor_drv\src\imx219\dcc_xmls\linear
quesion"
can i refer IMX219_linear 's XML,sensor for access to raw8?
Hi quan,
,Is the bit width of the data input to the LSC module incorrect?
It is more likely that LSC is not correctly tuned.
can i refer IMX219_linear 's XML,sensor for access to raw8
Of course you can.
HI:adam
With reference to the parameters of IMX219, the graph problem has not been solved.
Hi,
Sorry, what's the graph problem? Can you please provide more information?
Regards,
Brijesh