Hi experts
My software version is:
PDK-RTOS :processor-sdk-rtos-j721e-evm-08_06_00_12
PDK-LINUX:processor-sdk-linux-08_06_00
When the TDA4VM EVM board is started in eMMC boot0 mode, it is stuck at remoteproc remoteproc5: Booting fw image j7-main-r5f0_1-fw, size 302028
U-Boot SPL 2021.01-dirty (May 16 2024 - 16:41:40 +0800)
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev A
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar')
Trying to boot from MMC1
init_env from device 17 not supported!
Starting ATF on ARM64 core...
NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
NOTICE: BL31: Built : 22:56:45, Mar 3 2023
I/TC:
I/TC: OP-TEE version: 3.20.0 (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 Fri Mar 3 22:54
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar')
I/TC: HUK Initialized
I/TC: Activated SA2UL device
I/TC: Fixing SA2UL firewall owner for GP device
I/TC: Enabled firewalls for SA2UL TRNG device
I/TC: SA2UL TRNG initialized
I/TC: SA2UL Drivers initialized
I/TC: Primary CPU switching to normal world boot
U-Boot SPL 2021.01-dirty (May 16 2024 - 16:41:33 +0800)
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev A
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar')
Detected: J7X-BASE-CPB rev A
Detected: J7X-VSC8514-ETH rev E2
Trying to boot from MMC1
U-Boot 2021.01-dirty (May 16 2024 - 16:41:33 +0800)
SoC: J721E SR1.1 GP
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev A
DRAM: 4 GiB
Flash: 0 Bytes
MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1
Loading Environment from MMC... OK
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000
Detected: J7X-BASE-CPB rev A
Detected: J7X-VSC8514-ETH rev E2
cdns,sierra serdes@5000000: sierra probed
Net: eth0: ethernet@46000000port@1
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0(part 0) is current device
SD/MMC found on device 0
Failed to load 'boot.scr'
** Unrecognized filesystem type **
19079680 bytes read in 118 ms (154.2 MiB/s)
111990 bytes read in 11 ms (9.7 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 000000008fee1000, end 000000008fffffff ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
[ 0.000000] Linux version 5.10.162-g76b3e88d56 (oe-user@oe-host) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-3
[ 0.000000] Machine model: Texas Instruments K3 J721E SoC
[ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[ 0.000000] printk: bootconsole [ns16550a0] enabled
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a4000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a4100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a5000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a5000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a5100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a5100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node c66-dma-memory@a6000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node c66-memory@a6100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node c66-dma-memory@a7000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node c66-memory@a7100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node c71-dma-memory@a8000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node c71-memory@a8100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000ac000000, size 2 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-virtual-eth-queues@ac000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000ac200000, size 30 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-virtual-eth-buffers@ac200000, compatible id shared-dma-pool
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal [mem 0x0000000100000000-0x00000008ffffffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff]
[ 0.000000] node 0: [mem 0x000000009e800000-0x00000000a8ffffff]
[ 0.000000] node 0: [mem 0x00000000a9000000-0x00000000a9ffffff]
[ 0.000000] node 0: [mem 0x00000000aa000000-0x00000000abbfffff]
[ 0.000000] node 0: [mem 0x00000000abc00000-0x00000000abffffff]
[ 0.000000] node 0: [mem 0x00000000ac000000-0x00000000adffffff]
[ 0.000000] node 0: [mem 0x00000000ae000000-0x00000000ffffffff]
[ 0.000000] node 0: [mem 0x0000000880000000-0x00000008ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff]
[ 0.000000] cma: Reserved 512 MiB at 0x00000000e0000000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 22 pages/cpu s50392 r8192 d31528 u90112
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: EL2 vector hardening
[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[ 0.000000] CPU features: detected: Spectre-BHB
[ 0.000000] CPU features: detected: ARM erratum 1742098
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1032192
[ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.t
[ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] software IO TLB: mapped [mem 0x00000000dc000000-0x00000000e0000000] (64MB)
[ 0.000000] Memory: 3271300K/4194304K available (11200K kernel code, 1160K rwdata, 4300K rodata, 1856K init, 433K bss, 398716K reserved, 524288)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 960 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @880800000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x0000000880030000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000880040000
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000002] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.008423] Console: colour dummy device 80x25
[ 0.012984] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[ 0.023654] pid_max: default: 32768 minimum: 301
[ 0.028408] LSM: Security Framework initializing
[ 0.033161] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.040736] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.049548] rcu: Hierarchical SRCU implementation.
[ 0.054611] Platform MSI: msi-controller@1820000 domain created
[ 0.060852] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created
[ 0.070155] EFI services will not be available.
[ 0.074878] smp: Bringing up secondary CPUs ...
I/TC: Secondary CPU 1 initializing
I/TC: Secondary CPU 1 switching to normal world boot
[ 0.088111] Detected PIPT I-cache on CPU1
[ 0.088135] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000
[ 0.088146] GICv3: CPU1: using allocated LPI pending table @0x0000000880050000
[ 0.088182] CPU1: Booted secondary processor 0x0000000001 [0x411fd080]
[ 0.088230] smp: Brought up 1 node, 2 CPUs
[ 0.117575] SMP: Total of 2 processors activated.
[ 0.122380] CPU features: detected: 32-bit EL0 Support
[ 0.127635] CPU features: detected: CRC32 instructions
[ 0.141638] CPU: All CPU(s) started at EL2
[ 0.145832] alternatives: patching kernel code
[ 0.150843] devtmpfs: initialized
[ 0.159800] KASLR disabled due to lack of seed
[ 0.164443] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.174407] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[ 0.187229] pinctrl core: initialized pinctrl subsystem
[ 0.192878] DMI not present or invalid.
[ 0.197117] NET: Registered protocol family 16
[ 0.202310] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
[ 0.209613] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.217661] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.225965] thermal_sys: Registered thermal governor 'step_wise'
[ 0.225968] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.232537] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.246173] ASID allocator initialised with 65536 entries
[ 0.271014] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.277870] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.284716] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.291561] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.299012] cryptd: max_cpu_qlen set to 1000
[ 0.305114] k3-chipinfo 43000014.chipid: Family:J721E rev:SR2.0 JTAGID[0x1bb6402f] Detected
[ 0.313940] vsys_3v3: supplied by evm_12v0
[ 0.318299] vsys_5v0: supplied by evm_12v0
[ 0.323056] iommu: Default domain type: Translated
[ 0.328227] SCSI subsystem initialized
[ 0.332401] mc: Linux media interface: v0.10
[ 0.336780] videodev: Linux video capture interface: v2.00
[ 0.342415] pps_core: LinuxPPS API ver. 1 registered
[ 0.347486] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.356824] PTP clock support registered
[ 0.360846] EDAC MC: Ver: 3.0.0
[ 0.364659] FPGA manager framework
[ 0.368166] Advanced Linux Sound Architecture Driver Initialized.
[ 0.374756] clocksource: Switched to clocksource arch_sys_counter
[ 0.381079] VFS: Disk quotas dquot_6.6.0
[ 0.385109] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.394690] NET: Registered protocol family 2
[ 0.399425] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.407995] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
[ 0.416751] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.424951] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear)
[ 0.432747] TCP: Hash tables configured (established 32768 bind 32768)
[ 0.439545] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.446439] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.453836] NET: Registered protocol family 1
[ 0.458548] RPC: Registered named UNIX socket transport module.
[ 0.464611] RPC: Registered udp transport module.
[ 0.469415] RPC: Registered tcp transport module.
[ 0.474218] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.480799] NET: Registered protocol family 44
[ 0.485343] PCI: CLS 0 bytes, default 64
[ 0.489717] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
[ 0.500131] Initialise system trusted keyrings
[ 0.504758] workingset: timestamp_bits=46 max_order=20 bucket_order=0
[ 0.512867] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.519120] NFS: Registering the id_resolver key type
[ 0.524310] Key type id_resolver registered
[ 0.528581] Key type id_legacy registered
[ 0.532700] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.539548] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.547185] 9p: Installing v9fs 9p2000 file system support
[ 0.572567] Key type asymmetric registered
[ 0.576754] Asymmetric key parser 'x509' registered
[ 0.581753] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.589312] io scheduler mq-deadline registered
[ 0.593938] io scheduler kyber registered
[ 0.599682] pinctrl-single 4301c000.pinctrl: 94 pins, size 376
[ 0.605870] pinctrl-single 11c000.pinctrl: 173 pins, size 692
[ 0.614984] ti-pat 31010000.pat: Found PAT Rev 1.0 with 16384 pages
[ 0.621410] debugfs: Directory '31010000.pat' with parent 'regmap' already present!
[ 0.629392] ti-pat 31011000.pat: Found PAT Rev 1.0 with 16384 pages
[ 0.635818] debugfs: Directory '31011000.pat' with parent 'regmap' already present!
[ 0.643762] ti-pat 31012000.pat: Found PAT Rev 1.0 with 16384 pages
[ 0.650179] debugfs: Directory '31012000.pat' with parent 'regmap' already present!
[ 0.658108] ti-pat 31013000.pat: Found PAT Rev 1.0 with 2048 pages
[ 0.664433] debugfs: Directory '31013000.pat' with parent 'regmap' already present!
[ 0.672384] ti-pat 31014000.pat: Found PAT Rev 1.0 with 2048 pages
[ 0.678711] debugfs: Directory '31014000.pat' with parent 'regmap' already present!
[ 0.688446] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.696711] arm-smmu-v3 36600000.iommu: ias 48-bit, oas 48-bit (features 0x00001faf)
[ 0.704926] arm-smmu-v3 36600000.iommu: allocated 65536 entries for cmdq
[ 0.711960] arm-smmu-v3 36600000.iommu: allocated 32768 entries for evtq
[ 0.720357] arm-smmu-v3 36600000.iommu: msi_domain absent - falling back to wired irqs
[ 0.733500] brd: module loaded
[ 0.739941] loop: module loaded
[ 0.743676] megasas: 07.714.04.00-rc1
[ 0.749477] tun: Universal TUN/TAP device driver, 1.6
[ 0.754961] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 0.761366] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 0.767441] sky2: driver version 1.30
[ 0.771810] VFIO - User Level meta-driver version: 0.3
[ 0.777603] i2c /dev entries driver
[ 0.782115] sdhci: Secure Digital Host Controller Interface driver
[ 0.788439] sdhci: Copyright(c) Pierre Ossman
[ 0.793109] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.799546] ledtrig-cpu: registered to indicate activity on CPUs
[ 0.805903] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 0.813304] optee: probing for conduit method.
I/TC: Reserved shared memory is enabled
I/TC: Dynamic shared memory is enabled
I/TC: Normal World virtualization support is disabled
I/TC: Asynchronous notifications are disabled
[ 0.817867] optee: revision 3.20 (8e74d476)
[ 0.834268] optee: dynamic shared memory is enabled
[ 0.843731] optee: initialized driver
[ 0.848913] NET: Registered protocol family 17
[ 0.853527] 9pnet: Installing 9P2000 support
[ 0.857922] Key type dns_resolver registered
[ 0.862374] Loading compiled-in X.509 certificates
[ 0.876100] ti-sci 44083000.dmsc: ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar')
[ 0.939468] davinci-mcasp 2ba0000.mcasp: IRQ common not found
[ 0.947267] omap_i2c 40b00000.i2c: bus 0 rev0.12 at 100 kHz
[ 0.953342] omap_i2c 40b10000.i2c: bus 1 rev0.12 at 100 kHz
[ 0.959762] omap_i2c 42120000.i2c: bus 2 rev0.12 at 100 kHz
[ 0.966255] pca953x 3-0020: supply vcc not found, using dummy regulator
[ 0.973081] pca953x 3-0020: using no AI
[ 0.999634] pca953x 3-0022: supply vcc not found, using dummy regulator
[ 1.006436] pca953x 3-0022: using AI
[ 1.010709] gpio-480 (CTRL_PM_I2C_OE): hogged as output/high
[ 1.016686] gpio-481 (MCASP/TRACE_MUX_S0): hogged as output/low
[ 1.022928] gpio-482 (MCASP/TRACE_MUX_S1): hogged as output/high
[ 1.029422] omap_i2c 2000000.i2c: bus 3 rev0.12 at 400 kHz
[ 1.035879] omap_i2c 2010000.i2c: bus 4 rev0.12 at 400 kHz
[ 1.045745] omap_i2c 2020000.i2c: bus 5 rev0.12 at 400 kHz
[ 1.052045] pca953x 6-0020: supply vcc not found, using dummy regulator
[ 1.058875] pca953x 6-0020: using no AI
[ 1.087430] omap_i2c 2030000.i2c: bus 6 rev0.12 at 400 kHz
[ 1.093505] omap_i2c 2040000.i2c: bus 7 rev0.12 at 100 kHz
[ 1.099473] omap_i2c 2050000.i2c: bus 8 rev0.12 at 100 kHz
[ 1.105719] pca953x 9-0020: supply vcc not found, using dummy regulator
[ 1.112537] pca953x 9-0020: using no AI
[ 1.139085] omap_i2c 2060000.i2c: bus 9 rev0.12 at 400 kHz
[ 1.145551] ti-sci-intr bus@100000:bus@28380000:interrupt-controller2: Interrupt Router 137 domain created
[ 1.155541] ti-sci-intr bus@100000:interrupt-controller0: Interrupt Router 131 domain created
[ 1.164352] ti-sci-intr bus@100000:main-navss:interrupt-controller1: Interrupt Router 213 domain created
[ 1.174219] ti-sci-inta 33d00000.interrupt-controller: Interrupt Aggregator domain 209 created
[ 1.196287] j721e-pcie 2900000.pcie: host bridge /bus@100000/pcie@2900000 ranges:
[ 1.203964] j721e-pcie 2900000.pcie: IO 0x0010001000..0x0010010fff -> 0x0010001000
[ 1.212242] j721e-pcie 2900000.pcie: MEM 0x0010011000..0x0017ffffff -> 0x0010011000
[ 1.220519] j721e-pcie 2900000.pcie: IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[ 2.239878] j721e-pcie 2900000.pcie: PCI host bridge to bus 0000:00
[ 2.246315] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 2.251921] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] (bus address [0x10001000-0x10010fff])
[ 2.261612] pci_bus 0000:00: root bus resource [mem 0x10011000-0x17ffffff]
[ 2.268667] pci 0000:00:00.0: [104c:b00d] type 01 class 0x060400
[ 2.274806] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[ 2.284755] pci 0000:00:00.0: supports D1
[ 2.288849] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[ 2.294735] pci 0000:00:00.0: reg 0x224: [mem 0x00000000-0x003fffff 64bit]
[ 2.301761] pci 0000:00:00.0: VF(n) BAR0 space: [mem 0x00000000-0x00ffffff 64bit] (contains BAR0 for 4 VFs)
[ 2.313869] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 2.323994] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01
[ 2.330767] pci 0000:00:00.0: BAR 7: assigned [mem 0x10400000-0x113fffff 64bit]
[ 2.338240] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 2.343541] pcieport 0000:00:00.0: PME: Signaling with IRQ 68
[ 2.349905] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
[ 2.357572] j721e-pcie 2910000.pcie: IO 0x0018001000..0x0018010fff -> 0x0018001000
[ 2.365848] j721e-pcie 2910000.pcie: MEM 0x0018011000..0x001fffffff -> 0x0018011000
[ 2.374130] j721e-pcie 2910000.pcie: IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[ 3.382783] j721e-pcie 2910000.pcie: PCI host bridge to bus 0001:00
[ 3.389191] pci_bus 0001:00: root bus resource [bus 00-ff]
[ 3.394797] pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x18001000-0x18010fff])
[ 3.404666] pci_bus 0001:00: root bus resource [mem 0x18011000-0x1fffffff]
[ 3.411709] pci 0001:00:00.0: [104c:b00d] type 01 class 0x060400
[ 3.417848] pci_bus 0001:00: 2-byte config write to 0001:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[ 3.427776] pci 0001:00:00.0: supports D1
[ 3.431871] pci 0001:00:00.0: PME# supported from D0 D1 D3hot
[ 3.439837] pci 0001:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 3.449951] pci_bus 0001:01: busn_res: [bus 01-ff] end is updated to 01
[ 3.456719] pci 0001:00:00.0: PCI bridge to [bus 01]
[ 3.461997] pcieport 0001:00:00.0: PME: Signaling with IRQ 71
[ 3.468356] j721e-pcie 2920000.pcie: host bridge /bus@100000/pcie@2920000 ranges:
[ 3.476029] j721e-pcie 2920000.pcie: IO 0x4400001000..0x4400010fff -> 0x0000001000
[ 3.484307] j721e-pcie 2920000.pcie: MEM 0x4400011000..0x4407ffffff -> 0x0000011000
[ 3.492585] j721e-pcie 2920000.pcie: IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[ 4.503941] j721e-pcie 2920000.pcie: PCI host bridge to bus 0002:00
[ 4.510369] pci_bus 0002:00: root bus resource [bus 00-ff]
[ 4.515975] pci_bus 0002:00: root bus resource [io 0x20000-0x2ffff] (bus address [0x1000-0x10fff])
[ 4.525223] pci_bus 0002:00: root bus resource [mem 0x4400011000-0x4407ffffff] (bus address [0x00011000-0x07ffffff])
[ 4.535998] pci 0002:00:00.0: [104c:b00d] type 01 class 0x060400
[ 4.542137] pci_bus 0002:00: 2-byte config write to 0002:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[ 4.552065] pci 0002:00:00.0: supports D1
[ 4.556159] pci 0002:00:00.0: PME# supported from D0 D1 D3hot
[ 4.564168] pci 0002:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 4.574288] pci_bus 0002:01: busn_res: [bus 01-ff] end is updated to 01
[ 4.581056] pci 0002:00:00.0: PCI bridge to [bus 01]
[ 4.586335] pcieport 0002:00:00.0: PME: Signaling with IRQ 74
[ 4.593167] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:235
[ 4.603048] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled
[ 4.609808] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66346100, num_proxies:64
[ 4.618805] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[440,150] sci-dev-id:211
[ 4.628942] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled
[ 4.635704] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66346100, num_proxies:64
[ 4.643667] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 15, base_baud = 6000000) is a 8250
[ 4.653068] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 33, base_baud = 3000000) is a 8250
[ 4.661815] printk: console [ttyS2] enabled
[ 4.661815] printk: console [ttyS2] enabled
[ 4.670253] printk: bootconsole [ns16550a0] disabled
[ 4.670253] printk: bootconsole [ns16550a0] disabled
[ 4.680712] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 34, base_baud = 3000000) is a 8250
[ 4.689649] 2840000.serial: ttyS6 at MMIO 0x2840000 (irq = 35, base_baud = 3000000) is a 8250
[ 4.700402] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vdd-hba-supply regulator, assuming enabled
[ 4.710915] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vcc-supply regulator, assuming enabled
[ 4.721072] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq-supply regulator, assuming enabled
[ 4.731312] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq2-supply regulator, assuming enabled
[ 4.742463] scsi host0: ufshcd
[ 4.751572] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
[ 4.764238] cdns-ufshcd 4e84000.ufs: ufshcd_print_pwr_info:[RX, TX]: gear=[1, 1], lane[1, 1], pwr[SLOWAUTO_MODE, SLOWAUTO_MODE], rate = 0
[ 4.794760] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 4.803241] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[ 4.811547] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2 quirks:00000000
[ 4.824427] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[ 4.831638] cdns-ufshcd 4e84000.ufs: ufshcd_print_pwr_info:[RX, TX]: gear=[3, 3], lane[2, 2], pwr[FAST MODE, FAST MODE], rate = 2
[ 4.843268] cdns-ufshcd 4e84000.ufs: ufshcd_find_max_sup_active_icc_level: Regulator capability was not set, actvIccLevel=0
[ 4.843270] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[ 4.843663] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010a, freq:500000000, add_val:1 pps:0
[ 4.869264] scsi 0:0:0:49488: Well-known LUN TOSHIBA THGAF8G8T23BAILB 0300 PQ: 0 ANSI: 6
[ 4.877781] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010a, freq:200000000, add_val:4 pps:0
[ 4.886296] scsi 0:0:0:49476: Well-known LUN TOSHIBA THGAF8G8T23BAILB 0300 PQ: 0 ANSI: 6
[ 4.895120] cdns-ufshcd 4e84000.ufs: ufshcd_scsi_add_wlus: BOOT WLUN not found
[ 4.987725] mmc0: CQHCI version 5.10
[ 4.987778] davinci-mcasp 2ba0000.mcasp: IRQ common not found
[ 5.003450] vdd_mmc1: supplied by vsys_3v3
[ 5.008397] pca953x 4-0020: supply vcc not found, using dummy regulator
[ 5.015079] pca953x 4-0020: using no AI
[ 5.027316] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit
[ 5.043762] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc7100
[ 5.050600] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc7100
[ 5.057433] omap-mailbox 31f82000.mailbox: omap mailbox rev 0x66fc7100
[ 5.064253] omap-mailbox 31f83000.mailbox: omap mailbox rev 0x66fc7100
[ 5.071057] omap-mailbox 31f84000.mailbox: omap mailbox rev 0x66fc7100
[ 5.081704] ti-udma 285c0000.dma-controller: Channels: 26 (tchan: 13, rchan: 13, gp-rflow: 8)
[ 5.092299] ti-udma 31150000.dma-controller: Channels: 122 (tchan: 61, rchan: 61, gp-rflow: 16)
[ 5.107065] spi-nor spi7.0: mt35xu512aba (65536 Kbytes)
[ 5.112297] 8 cmdlinepart partitions found on MTD device 47040000.spi.0
[ 5.118905] Creating 8 MTD partitions on "47040000.spi.0":
[ 5.124384] 0x000000000000-0x000000080000 : "ospi.tiboot3"
[ 5.130364] 0x000000080000-0x000000280000 : "ospi.tispl"
[ 5.136058] 0x000000280000-0x000000680000 : "ospi.u-boot"
[ 5.141831] 0x000000680000-0x0000006c0000 : "ospi.env"
[ 5.147378] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw"
[ 5.153058] 0x0000007c0000-0x000000800000 : "ospi.env.backup"
[ 5.159180] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
[ 5.164964] 0x000003fc0000-0x000004000000 : "ospi.phypattern"
[ 5.173931] spi-nor spi8.0: mt25qu512a (65536 Kbytes)
[ 5.180576] mmc0: Command Queue Engine enabled
[ 5.180917] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
[ 5.185026] mmc0: new HS200 MMC card at address 0001
[ 5.196881] mmcblk0: mmc0:0001 S0J56X 14.8 GiB
[ 5.201517] mmcblk0boot0: mmc0:0001 S0J56X partition 1 31.5 MiB
[ 5.207532] mmcblk0boot1: mmc0:0001 S0J56X partition 2 31.5 MiB
[ 5.213527] mmcblk0rpmb: mmc0:0001 S0J56X partition 3 4.00 MiB, chardev (237:0)
[ 5.223366] mmcblk0: p1
[ 5.230771] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 5.239263] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[ 5.247571] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2 quirks:00000000
[ 5.260376] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[ 5.267581] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[ 5.273837] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010a, freq:500000000, add_val:1 pps:0
[ 5.284140] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[ 5.292482] davinci-mcasp 2ba0000.mcasp: IRQ common not found
[ 5.298673] mmc1: CQHCI version 5.10
[ 5.308436] debugfs: Directory 'pd:27' with parent 'pm_genpd' already present!
[ 5.315690] debugfs: Directory 'pd:26' with parent 'pm_genpd' already present!
[ 5.324049] debugfs: Directory 'pd:242' with parent 'pm_genpd' already present!
[ 5.331366] debugfs: Directory 'pd:241' with parent 'pm_genpd' already present!
[ 5.338677] debugfs: Directory 'pd:240' with parent 'pm_genpd' already present!
[ 5.345988] debugfs: Directory 'pd:239' with parent 'pm_genpd' already present!
[ 5.354376] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[ 5.375639] ALSA device list:
[ 5.378600] No soundcards found.
[ 6.819416] sdhci-am654 4fb0000.mmc: Power on failed
[ 6.854995] mmc1: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 64-bit
[ 6.888260] EXT4-fs (mmcblk0p1): recovery complete
[ 6.893778] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Opts: (null)
[ 6.901888] VFS: Mounted root (ext4 filesystem) on device 179:1.
[ 6.908971] devtmpfs: mounted
[ 6.912766] Freeing unused kernel memory: 1856K
[ 6.917391] Run /sbin/init as init process
[ 6.985779] systemd[1]: System time before build time, advancing clock.
[ 7.012066] NET: Registered protocol family 10
[ 7.016965] Segment Routing with IPv6
[ 7.031905] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRY)
[ 7.053708] systemd[1]: Detected architecture arm64.
Welcome to Arago 2021.09!
[ 7.099179] systemd[1]: Set hostname to <j7-evm>.
[ 7.222256] systemd[1]: /lib/systemd/system/irqbalanced.service:6: Unknown key name 'ConditionCPUs' in section 'Unit', ignoring.
[ 7.243430] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= references a path below legacy directory /var/run/, updating /var/ru.
[ 7.299199] random: systemd: uninitialized urandom read (16 bytes read)
[ 7.307452] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 7.326834] random: systemd: uninitialized urandom read (16 bytes read)
[ 7.334234] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 7.354829] random: systemd: uninitialized urandom read (16 bytes read)
[ 7.362074] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 7.382953] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password …ts to Console Directory Watch.
[ 7.406877] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R…uests to Wall Directory Watch.
[ 7.430871] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 7.450826] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 7.470812] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 7.490818] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 7.521245] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 7.542884] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 7.567175] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ 7.586985] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 7.612322] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[ 7.620659] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 7.643076] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 7.663112] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 7.687017] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 7.706957] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 7.728932] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 7.752966] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 7.777016] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 7.803164] systemd[1]: Mounting Temporary Directory (/tmp)...
Mounting Temporary Directory (/tmp)...
[ 7.825213] systemd[1]: Starting Create list of static device nodes for the current kernel...
Starting Create list of st…odes for the current kernel...
[ 7.855279] systemd[1]: Starting Start psplash boot splash screen...
Starting Start psplash boot splash screen...
[ 7.881091] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 7.898957] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[ 7.910995] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 7.935247] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 7.948914] cryptodev: loading out-of-tree module taints kernel.
[ 7.957267] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 7.971662] EXT4-fs (mmcblk0p1): re-mounted. Opts: (null)
[ 7.977204] cryptodev: driver 1.10 loaded.
[ 7.984198] systemd[1]: Starting udev Coldplug all Devices...
Starting udev Coldplug all Devices...
[ 8.009886] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 8.027260] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Started Create list of sta… nodes for the current kernel.
[FAILED] Failed to start Start psplash boot splash screen.
See 'systemctl status psplash-start.service' for details.
[DEPEND] Dependency failed for Star…progress communication helper.
[ OK ] Started Load Kernel Modules.
[ OK ] Started Remount Root and Kernel File Systems.
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
[ 8.247801] systemd-journald[183]: Received client request to flush runtime journal.
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev...
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ 8.355379] random: systemd: uninitialized urandom read (16 bytes read)
[ OK ] Reached target Local File Systems (Pre).
[ 8.378936] random: systemd: uninitialized urandom read (16 bytes read)
Mounting /media/ram...
[ 8.391136] random: systemd-journal: uninitialized urandom read (16 bytes read)
Mounting /var/volatile...
Starting udev Kernel Device Manager...
[ OK ] Started udev Coldplug all Devices.
[ OK ] Mounted /media/ram.
[ OK ] Mounted /var/volatile.
[ OK ] Started udev Kernel Device Manager.
Starting udev Wait for Complete Device Initialization...
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Network Time Synchronization.
[ 8.725471] random: crng init done
[ 8.730118] random: 64 urandom warning(s) missed due to ratelimiting
[ OK ] Started Load/Save Random Seed.
[ OK ] Reached target System Time Set.
[ OK ] Reached target System Time Synchronized.
[ 8.791430] ina2xx 5-0040: power monitor ina226 (Rshunt = 10000 uOhm)
[ 8.804861] ina2xx 5-0041: power monitor ina226 (Rshunt = 10000 uOhm)
[ 8.814548] ina2xx 5-0042: power monitor ina226 (Rshunt = 10000 uOhm)
[ 8.823493] ina2xx 5-0043: power monitor ina226 (Rshunt = 10000 uOhm)
[ 8.835561] ina2xx 5-0044: power monitor ina226 (Rshunt = 10000 uOhm)
[ 8.842992] CAN device driver interface
[ 8.872378] ina2xx 5-0045: power monitor ina226 (Rshunt = 5000 uOhm)
[ 8.892418] ina2xx 5-0046: power monitor ina226 (Rshunt = 10000 uOhm)
[ 8.929223] ina2xx 5-0047: power monitor ina226 (Rshunt = 10000 uOhm)
[ 8.940223] ina2xx 5-0048: power monitor ina226 (Rshunt = 10000 uOhm)
[ 8.947242] img_enc 4200000.video-encoder: vxe_enc_probe: using heap 1 for internal alloc
[ 8.966638] img_enc 4200000.video-encoder: encoder registered as /dev/video0
[ 8.973884] img_dec 4300000.video-decoder: decoder registered as /dev/video1
[ 8.981629] ina2xx 5-0049: power monitor ina226 (Rshunt = 10000 uOhm)
[ 8.989283] ina2xx 5-004a: power monitor ina226 (Rshunt = 10000 uOhm)
[ 8.998220] ina2xx 5-004b: power monitor ina226 (Rshunt = 10000 uOhm)
[ 9.008535] ina2xx 5-004c: power monitor ina226 (Rshunt = 10000 uOhm)
[ 9.016335] ina2xx 5-004d: power monitor ina226 (Rshunt = 10000 uOhm)
[ 9.026952] ina2xx 5-004e: power monitor ina226 (Rshunt = 10000 uOhm)
[ 9.034653] k3-dsp-rproc 4d80800000.dsp: assigned reserved memory node c66-dma-memory@a7000000
[ 9.045020] ina2xx 5-004f: power monitor ina226 (Rshunt = 10000 uOhm)
[ 9.053534] k3-dsp-rproc 4d80800000.dsp: configured DSP for remoteproc mode
[ 9.062712] k3-dsp-rproc 4d80800000.dsp: local reset is deasserted for device
[ 9.074260] remoteproc remoteproc0: 4d80800000.dsp is available
[ 9.083650] k3-dsp-rproc 4d81800000.dsp: assigned reserved memory node c66-dma-memory@a6000000
[ 9.097490] k3-dsp-rproc 4d81800000.dsp: configured DSP for remoteproc mode
[ 9.105076] remoteproc remoteproc0: powering up 4d80800000.dsp
[ 9.110983] remoteproc remoteproc0: Booting fw image j7-c66_0-fw, size 1334036
[ 9.118734] remoteproc remoteproc0: bad phdr da 0xa8100000 mem 0x8c
[ 9.120210] platform 41000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[ 9.125010] remoteproc remoteproc0: Failed to load program segments: -22
[ 9.150369] k3-dsp-rproc 4d81800000.dsp: local reset is deasserted for device
[ 9.160152] platform 41000000.r5f: configured R5F for IPC-only mode
[ 9.173869] remoteproc remoteproc1: 4d81800000.dsp is available
[ 9.183437] k3-dsp-rproc 64800000.dsp: assigned reserved memory node c71-dma-memory@a8000000
[ 9.192964] [drm] Initialized tidss 1.0.0 20180215 for 4a00000.dss on minor 0
[ 9.200696] remoteproc remoteproc1: powering up 4d81800000.dsp
[ 9.201502] platform 41000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000
[ 9.208056] remoteproc remoteproc1: Booting fw image j7-c66_1-fw, size 1334036
[ 9.216063] remoteproc remoteproc2: 41000000.r5f is available
[ 9.222546] tidss 4a00000.dss: [drm] Cannot find any crtc or sizes
[ 9.229075] remoteproc remoteproc2: attaching to 41000000.r5f
[ 9.236579] pvrsrvkm 4e20000000.gpu: More than one power domain for this GPU, gpu driver manages power domains
[ 9.242312] platform 41000000.r5f: R5F core initialized in IPC-only mode
[ 9.256500] remoteproc remoteproc1: bad phdr da 0xa9100000 mem 0x8c
[ 9.262896] remoteproc remoteproc1: Failed to load program segments: -22
[ 9.269792] remoteproc2#vdev0buffer: assigned reserved memory node r5f-dma-memory@a0000000
[ 9.279150] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 9.279467] k3-dsp-rproc 64800000.dsp: configured DSP for remoteproc mode
[ 9.285123] remoteproc2#vdev0buffer: registered virtio0 (type 7)
[ 9.291614] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
[ 9.297547] remoteproc remoteproc2: remote processor 41000000.r5f is now attached
[ 9.313943] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
[ 9.314208] remoteproc remoteproc3: 64800000.dsp is available
[ 9.331292] PVR_K: 219: Read BVNC 22.104.208.318 from HW device registers
[ 9.360118] platform 5c00000.r5f: configured R5F for remoteproc mode
[ 9.374804] remoteproc remoteproc3: powering up 64800000.dsp
[ 9.380473] remoteproc remoteproc3: Booting fw image j7-c71_0-fw, size 12849048
[ 9.388594] remoteproc remoteproc3: unsupported resource 65538
[ 9.394474] remoteproc remoteproc3: bad phdr da 0xb2100000 mem 0x98
[ 9.395675] PVR_K: 219: RGX Device registered with BVNC 22.104.208.318
[ 9.401812] remoteproc remoteproc3: Failed to load program segments: -22
[ 9.411056] platform 5c00000.r5f: assigned reserved memory node r5f-dma-memory@a2000000
[ 9.537051] remoteproc remoteproc4: 5c00000.r5f is available
[ 9.550843] [drm] Initialized pvr 1.15.6133109 20170530 for 4e20000000.gpu on minor 1
[ 9.594952] platform 5d00000.r5f: configured R5F for remoteproc mode
[ 9.607124] remoteproc remoteproc4: powering up 5c00000.r5f
[ 9.612890] remoteproc remoteproc4: Booting fw image j7-main-r5f0_0-fw, size 1424760
[ 9.628453] remoteproc remoteproc4: bad phdr da 0xa2104000 mem 0x1687b70
[ 9.638792] remoteproc remoteproc4: Failed to load program segments: -22
[ 9.679195] platform 5d00000.r5f: assigned reserved memory node r5f-dma-memory@a3000000
[ 9.771319] m_can_platform 40528000.can: m_can device registered (irq=23, version=32)
[ 9.772171] remoteproc remoteproc5: 5d00000.r5f is available
[ 9.791675] m_can_platform 40568000.can: m_can device registered (irq=25, version=32)
[ 9.792385] remoteproc remoteproc5: powering up 5d00000.r5f
[ 9.807026] remoteproc remoteproc5: Booting fw image j7-main-r5f0_1-fw, size 302028
[ 9.816187] m_can_platform 2701000.can: m_can device registered (irq=55, version=32)
[ 9.852083] platform 5e00000.r5f: configured R5F for remoteproc mode
Please help us solve it, thanks
Regards,
Barry