Part Number: AM62A7-Q1
HI TI:
How can I generate a cac LUT file when I have the following lens information。

If it cannot be generated, what other lens information needs to be provided? Thank you very much
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM62A7-Q1
HI TI:
How can I generate a cac LUT file when I have the following lens information。

If it cannot be generated, what other lens information needs to be provided? Thank you very much
Hi yangrongbo,
CAC can undo shifts on R and B pixels relative to G pixels.
You may follow the FAQ below for generating CAC tuning with DCC tuning tool.
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1283047/faq-tda4vh-am62a-how-to-create-the-cac-mesh-lut-for-dcc-tuning-tool-input
It looks like you have some data on relative radial shifts between certain wavelength.
For example, 470nm to 550nm shifts may be close to R-G shifts, but won't be exact and may change with lighting.
We don't have much experience about how to use these measurement data and you will have to experiment on that.
HI Gang Hua:
There are still issues after CAC. Also, I don't think CAC can solve this problem. I tested ISX031 (with the same lens model and sensor), and there was no color difference in the middle area and no CAC was done. As shown in the figure:


Hi Yang,
I see color difference in the raw you emailed. I don't think it is an issue can be solved from ISP. It is better to contact Sony on this issue.

https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/image_5F00_v17_2D00_35.raw
Regards,
Adam
Hi yangrongbo,
There are still issues after CAC. Also, I don't think CAC can solve this problem.
As we discussed on another thread, there are 2 possible causes for this kind of artifacts.
(1) CA if you the issue does not appear on image center, but around image corner.
Do you have the sample raw/yuv images for both?
(2) WDR tone mapping around bright lights.
This one we would have to check if it is a problem in sensor WDR merge or ISP WDR tone mapping.
Yes,
I see color difference in the raw you emailed.
Yes, I also see the same color artifacts (should be due to strong aliasing) in the raw image after linearization.
It is difficult for TDA4 ISP to remove this type of color artifacts.