This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5748: How to add Hardware flow control in SYS/BIOS UART example for AM57xx.

Part Number: AM5748

Tool/software:

Hi ,

              We are trying to enable HW flow control in AM5748 UART SYS/BIOS example , when I checked uartParams structure in UART.h driver include file, there we need to define a Macro  to  enable the HW flow control.

-------------------------------------------------------------------------------------------------------------

#ifdef PRU_ICSS_FW // PRU UART FW only, currently unsupported by HW IP driver
UART_FC_TYPE flowControlType; /*!< Flow Control type */
uint8_t hwFlowControlThr; /*!< Hardware flow Control threshold, 0-0x100 */
#endif

-------------------------------------------------------------------------------------------------------------

We have copied the UART.h and UART_drv.c file locally in our project and enabled this PRU_ICSS_FW macro, still when we observed the the signals in scope there is no activity in RTS and CTS, it's working like a Normal UART.

So, we need your support regarding enabling the HW flow control.

Thanks ,

Phaneesh A