Hallo TI Community,
I am working on an TI-RTOS application where I need to use the hardware flow control functionality of my UART serial interfaces. The problem is that I didn't find any information (neither API functions nor parameters) says that UART.h API supports hardware flow control (CTS/RTS), however my AM5726 technical reference manual states that it supports UART HW flow control (CTS/RTS). I found other implemented drivers with HW flow control which are developed for other platforms like (UARTCC26XX.h, UARTTiva.h,..) but not for AM5726.
- Is there any implemented UART driver in TI-RTOS that supports HW control for AM5726?
Thanks,
Ziad