This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: EtherCAT coupler design suggestions

Part Number: AM6442
Other Parts Discussed in Thread: TMDS64EVM

Tool/software:

Hi Expert,

1.Are the hardware circuits the same in industrial communication applications?

2.Does it support CC-Link IE?

3.Is there a suggested EVM or reference design?

Thanks

Daniel

  • Hi Daniel,

    Please see below:

    #1: Not sure I understand your question. For Slave protocol support, you need to use the ICSSG modules (not the CPSW Etherent ports); You must alos purchze Device Option "E"

    #2:Yes, the device can suppot CC-Link slave, but you will need to work with a 3rd party for the software (TI does not provide it)

    #3: Please use the TMDS64EVM whcih suppots the industrial communicaion protocols. 

    Device_Options.pptx