Tool/software:
Encoders: id crtc type possible crtcs possible clones 39 0 DPI 0x00000001 0x00000001 Connectors: id encoder status name size (mm) modes encoders 40 0 connected DPI-1 97x54 1 39 modes: index name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot #0 800x480 20.79 800 801 802 887 480 481 484 488 9000 flags: nhsync, nvsync; type: preferred, driver .................... CRTCs: id fb pos size 38 0 (0,0) (0x0) #0 nan 0 0 0 0 0 0 0 0 0 flags: ; type: props: 24 VRR_ENABLED: flags: range
How is the value 20.79 of the refresh (Hz) property in the code above set?
Are there any Register settings?