This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS64EVM: Run DDR4 at highest clock frequency

Part Number: TMDS64EVM

Tool/software:

Hello TI,

as per our requirement we would like to run ddr4 RAM at highest clock frequency.i.e 800MHz as per the datasheet.

I was check with current frequency with k3conf dump clock 138 it is showing below.

root@am64xx-evm:~# k3conf dump clock 138
|------------------------------------------------------------------------------|
| VERSION INFO                                                                 |
|------------------------------------------------------------------------------|
| K3CONF | (version 0.3-nogit built Sun Mar 03 08:52:05 UTC 2024)              |
| SoC    | AM64x SR2.0                                                         |
| SYSFW  | ABI: 3.1 (firmware version 0x0009 '9.2.7--v09.02.07 (Kool Koala))') |
|------------------------------------------------------------------------------|

|-------------------------------------------------------------------------------------------|
| Device ID | Clock ID | Clock Name                     | Status          | Clock Frequency |
|-------------------------------------------------------------------------------------------|
|   138     |     0    | DEV_DDR16SS0_DDRSS_DDR_PLL_CLK | CLK_STATE_READY | 400000000       |
|   138     |     1    | DEV_DDR16SS0_PLL_CTRL_CLK      | CLK_STATE_READY | 500000000       |

how to run DDR4 at highest frequency in linux,we are using TMDS64 evm and Debian bookwarm processor sdk of version .09.02.09