This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] How to enable switching capability between GPO and GPI operation for PRU GPIO?

Part Number: AM6442
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

Each PRU_ICSSG PRU processor implements fast GPO through its R30 register and fast GPI through R31 register. AM64x/AM243x has 20 pinned out PRU GPIO pins and the device multiplexes all GPI signals and their corresponding GPO signals onto the same pin using different multiplexing modes.

How to switch between GPO and GPI operation from PRU firmware code?

  • PRU GPIO Bidirectional mode for AM64x and AM243x

    We can program the PRU GPIO pins in bidirectional mode to enable switching between GPO and GPI operation from PRU. Special I/O pin connectivity for the GPO/GPI pins is implemented using the IEP EDIO signal controls to provide input/output switching using a single SoC level pin multiplexing mode.

    The IEP EDIO interface has 32 data output enable (DATA_OUT_EN) signals corresponding to its 32 data input and 32 data output signals. On the device, only 4 of the IEP0 EDIO (and none of the IEP1 EDIO) I/Os of each PRU_ICSSG module are pinned out (PRG[2:0]_IEP0_EDIO_DATA_IN_OUT[31:28]). 

    The unused output enables can be optionally re-purposed as GPO enables allowing each ICSSG GP pin to function as either a GPO or as a GPI when the I/O pin is configured for the GPO muxmodeA set of SoC level registers (CTRLMMR_ICSSG[2:0]_CTRL[2:0]) are used to determine the behavior of each GPO mode pin.

    By default, the [19-0]GPM_BIDI bit field is set to 0h and the corresponding GPO pins operate only as an output when the GPO muxmode is selected. The corresponding GPI signal (ICSSG GPI[19:0] input) is driven low.

    When a register’s [19-0]GPM_BIDI bit field is set to 1h, the corresponding ICSSG_DIGIO_DATA_OUT_EN_REG[31-0] DATA_OUT_EN bit field is used to control the GPO output buffer.

    • If [31-0] DATA_OUT_EN bit field is set to 0h, output is driven and the pin acts as a GPO.
    • If [31-0] DATA_OUT_EN bit field is set to 1h, output is disabled and the pin acts as a GPI.
  • Steps to enable bidirectional mode in PRU IO Empty project:

    Import CCS projects-

    1. Browse to the directory mcu_plus_sdk/examples/pru_io/empty/
    2. Import the R5F project (empty_pru_io_am64x-evm_r5fss0-0_freertos_ti-arm-clang) and PRU project (empty_am64x-evm_icssg0-pru0_fw_ti-pru-cgt) into CCS.

    Modifications to the R5F project-

    1. Open sysconfig and add a PRU (ICSS) instance present under TI Drivers.
    2. In the new added instance, go to 'Additional ICSS settings' > 'PRU (ICSS) GPIO' and add a new element to PRU (ICSS) GPIO.
    3. Select the GPO signals you want to work on and make sure to check the ‘Rx’ option with the GPO pins to ensure Rx is enable when they are changed to GPI.


    4. Save the configuration.
  • Modifications to the PRU project-

    Below code enables bidirectional functionality for PRU GPIO[6-0] and converts GPO3 to GPI3. Replace the code present after clearing the register space (zero &r0, 120) in main.asm file with the following.

    1. CTRL_MMR0 module has a protection mechanism (LOCKi_KICK0 and LOCKi_KICK1 registers) to prevent spurious writes from changing the registers.values. The process to unlock the protection mechanism are documented here -  TRM section 5.1.1.3.1.2 Kick Protection Registers.

      Fullscreen
      1
      2
      3
      4
      5
      6
      7
      8
      9
      10
      11
      12
      13
      14
      15
      16
      17
      PIN_CONTROL:
      ;Unlock CTRLMMR kick protection registers
      ldi32 TEMP_REG, 0x68EF3490
      ldi32 CTRL_REG, 0x43001008
      sbbo &TEMP_REG, CTRL_REG, 0, 4
      ldi32 TEMP_REG, 0xD172BC5A
      ldi32 CTRL_REG, 0x4300100C
      sbbo &TEMP_REG, CTRL_REG, 0, 4
      ldi32 TEMP_REG, 0x68EF3490
      ldi32 CTRL_REG, 0x43005008
      sbbo &TEMP_REG, CTRL_REG, 0, 4
      ldi32 TEMP_REG, 0xD172BC5A
      ldi32 CTRL_REG, 0x4300500C
      sbbo &TEMP_REG, CTRL_REG, 0, 4
      XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX


    2. Any GPO (Muxmode 0 function) can be made bidirectional by setting the corresponding bit field [19-0]GPM_BIDI in CTRLMMR_ICSSG[2:0]_CTRL[2:0] register.

      Fullscreen
      1
      2
      3
      4
      ;Set bits 0-6 of CTRLMMR_ICSSG0_CTRL0 to 1 to enable PRU fast GPIO as bidirectional
      ldi32 TEMP_REG, 0x7F
      ldi32 CTRL_REG, 0x43004100
      sbbo &TEMP_REG, CTRL_REG, 0, 4
      XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX


    3. Setting [31-0] DATA_OUT_EN bit field to 1h disables the output and the pin acts as a GPI.

      Fullscreen
      1
      2
      3
      4
      5
      6
      ;Set bits in IEP_DIGIO_DATA_OUT_EN_REG, GPIO 3 to inputs, rest as outputs
      ldi32 TEMP_REG, 0x08
      ldi32 EN_REG, 0x2e314
      sbbo &TEMP_REG, EN_REG, 0, 4
      halt ;end of program
      XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX


    Build and run the example-

    Follow the steps here - EXAMPLES_PRU_EMPTY to build and run the example

    Test the functionality -

    Set one of the GPO pins high by writing 1h to the corresponding R30 register bit and externally loop it to GPI3. As a result, value of the R31 register should change on receiving the high signal in GPI3.

  • Additional Note: Unlocking the CTRLMMR protection mechanism and bidirectional configuration is a one time setup and can be added on R5F side as below.

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    15
    16
    17
    18
    19
    20
    21
    #define KICK0_UNLOCK_VAL (0x68EF3490U)
    #define KICK1_UNLOCK_VAL (0xD172BC5AU)
    #define CSL_MAIN_LOCK0_KICK0_OFFSET (0x1008)
    #define CSL_MAIN_LOCK1_KICK0_OFFSET (0x5008)
    void config_CTRLMMR()
    {
    uint32_t baseAddr;
    volatile uint32_t *kickAddr;
    volatile uint32_t *regAddr = (volatile uint32_t *)((uint32_t)0x43004100);
    baseAddr = (uint32_t)(0x43000000);
    /* Lock 0 */
    kickAddr = (volatile uint32_t *) (baseAddr + CSL_MAIN_LOCK0_KICK0_OFFSET);
    CSL_REG32_WR(kickAddr, KICK0_UNLOCK_VAL); /* KICK 0 */
    kickAddr++;
    CSL_REG32_WR(kickAddr, KICK1_UNLOCK_VAL); /* KICK 1 */
    /* Lock 1 */
    kickAddr = (volatile uint32_t *) (baseAddr + CSL_MAIN_LOCK1_KICK0_OFFSET);
    CSL_REG32_WR(kickAddr, KICK0_UNLOCK_VAL); /* KICK 0 */
    kickAddr++;
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

  • Attached below are the modified PRU IO empty project files with bidirectional mode enabled for PRU GPIO.

    pru_gpio_bidirectional_mode_enable_projects.zip