Tool/software:
Champs:
As the title, My customer PCB is not able to boot okay with SDK8.02.
But the SDK8.6 is totally okay.
The Boot fail log with 9.02 SDK is the below.
Is this E2E the solution to fix my issue?
e2e.ti.com/.../am625-q1-u-boot-kernel-porting
BR Rio
U-Boot SPL 2023.04-ti-g836606420854 (May 09 2024 - 05:42:45 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.8--v09.02.08 (Kool Koala)')
SPL initial stack usage: 13408 bytes
Trying to boot from MMC2
Authentication passed
Authentication passed
Authentication passed
Authentication passed
Authentication passed
Starting ATF on ARM64 core...
NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty
NOTICE: BL31: Built : 16:09:05, Feb 9 2024
U-Boot SPL 2023.04-ti-g836606420854 (May 09 2024 - 05:42:45 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.8--v09.02.08 (Kool Koala)')
SPL initial stack usage: 1856 bytes
i2c_write: error waiting for data ACK (status=0x116)
pca953x gpio@22: Error reading output register
Card did not respond to voltage select! : -110
** Bad device specification mmc 1 **
Couldn't find partition mmc 1:1
Error: could not access storage.
Trying to boot from MMC2
i2c_write: error waiting for data ACK (status=0x116)
pca953x gpio@22: Error reading output register
Card did not respond to voltage select! : -110
spl: mmc init failed with error: -95
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###