Other Parts Discussed in Thread: TMS320C5533
Can you confirm the number of simultaneously active communication buses on the TMS320C5533:
There are 4 I2S ports. One of the I2S ports (set of pins) is shared with a SPI set of pins (P11, P9, P5, N10). However, the BGA pins for the 5533 show a second set of SPI pins (K1, L3, N4, L1) that are not shared with an I2S port.
Please confirm that the SPI port on the separated pins (K1, L3, N4, L1) can be used simultaneously with I2S activity on the 4 I2S ports (i.e. all 5 ports running).