Part Number: AM62A7
Tool/software:
Hi teams,
I want to use watchdog to callback my own function to save some information to log , in sdk9.2 I patched the follow code
ref : e2e.ti.com/.../am62a7-enabling-the-watchdog-and-testing
--- a/arch/arm64/boot/dts/ti/k3-am62a-main.dtsi
+++ b/arch/arm64/boot/dts/ti/k3-am62a-main.dtsi
@@ -795,6 +795,42 @@ main_mcan0: can@20701000 {
status = "disabled";
};
+ main_rti0: watchdog@e000000 {
+ compatible = "ti,j7-rti-wdt";
+ reg = <0x00 0x0e000000 0x00 0x100>;
+ clocks = <&k3_clks 125 0>;
+ power-domains = <&k3_pds 125 TI_SCI_PD_EXCLUSIVE>;
+ assigned-clocks = <&k3_clks 125 0>;
+ assigned-clock-parents = <&k3_clks 125 2>;
+ };
+
+ main_rti1: watchdog@e010000 {
+ compatible = "ti,j7-rti-wdt";
+ reg = <0x00 0x0e010000 0x00 0x100>;
+ clocks = <&k3_clks 126 0>;
+ power-domains = <&k3_pds 126 TI_SCI_PD_EXCLUSIVE>;
+ assigned-clocks = <&k3_clks 126 0>;
+ assigned-clock-parents = <&k3_clks 126 2>;
+ };
+
+ main_rti2: watchdog@e020000 {
+ compatible = "ti,j7-rti-wdt";
+ reg = <0x00 0x0e020000 0x00 0x100>;
+ clocks = <&k3_clks 127 0>;
+ power-domains = <&k3_pds 127 TI_SCI_PD_EXCLUSIVE>;
+ assigned-clocks = <&k3_clks 127 0>;
+ assigned-clock-parents = <&k3_clks 127 2>;
+ };
+
+ main_rti3: watchdog@e030000 {
+ compatible = "ti,j7-rti-wdt";
+ reg = <0x00 0x0e030000 0x00 0x100>;
+ clocks = <&k3_clks 128 0>;
+ power-domains = <&k3_pds 128 TI_SCI_PD_EXCLUSIVE>;
+ assigned-clocks = <&k3_clks 128 0>;
+ assigned-clock-parents = <&k3_clks 128 2>;
+ };
+
epwm0: pwm@23000000 {
compatible = "ti,am64-epwm", "ti,am3352-ehrpwm";
#pwm-cells = <3>;
/dev/watchdog can be seen ,
In bootloader cmdline :
=> mw.l 0xe0000a4 0xa 1 => mw.l 0xe000090 0xA98559DA 1
nothing happend , the board not reset,
In linux:
/opt/ltp/runltp -P am64xx-evm -f ddt/wdt_test -s WDT_S_FUNC_GETSTATUS
evm board not reset,
but I can see the address value
My requirement is that the watchdog can call back to my own function to record logs.
Is this function possible? How to do it , please help us.