Other Parts Discussed in Thread: SK-AM62A-LP, SK-AM62P-LP, AM62P, SK-AM62-LP
Tool/software:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello Libin,
Yes, the V3Link deserializer board can work with SK-AM62P-LP. You can simply download the Processor SDK Linux for AM62P and build this overlay: https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/tree/arch/arm64/boot/dts/ti/k3-am62x-sk-csi2-v3link-fusion.dtso?h=ti-linux-6.1.y.
Are you going to use IMX219? Please keep in mind that AM62P doesn't have an ISP and won't work with IMX219.
Regards,
Jianzhong
Dear Jianzhong,
Ok. I understand.
Yes, the set from Arducam has IMX219 and was brought as a package. Anyways, did you mean that we cannot use IMX219 even for video feed?
If not for IMX219, could you kindly suggest a camera and it serializer for Sk-am62-lp (AM62P)
Best regards
Libin Jose
Anyways, did you mean that we cannot use IMX219 even for video feed?
You can still capture raw images from IMX219, but won't be able to stream the images to a display or for other purposes.
If not for IMX219, could you kindly suggest a camera and it serializer for Sk-am62-lp (AM62P)
We've tested the OV5640 camera modules from Technexion https://www.technexion.com/products/embedded-vision/image-sensors/tevi-ov5640/ on AM62P.
Regards,
Jianzhong
Dear Jianzhong
Please confirm the module.
https://www.technexion.com/shop/embedded-vision/fpd-link/uvli-ov5640-c-s84-ir/
Thanks in advance.
Best regards
Libin Jose.
The link you provided is an FPDlink based camera. Please use the link that I provided.
Dear Jianzhong,
Our requirement is to connect 4 cameras through a serdes adapter and implement surround view system.
So we need 4 cameras with FAKRA connecter connected to adapter board and to am62p through MIPI-CSI2.
Could you kindly suggest any such adapter with camera?
Best regards
Libin Jose.
Hello Libin,
Please purchase the V3link camera kit from Arducam: https://www.arducam.com/product/arducam-v3link-camera-kit-for-ti-development-boards/. Then buy 4 OV5640 cameras with 120 degree FOV from Arducam (please contact their sales department for these cameras as they are not yet available on their website).
After you get these, replace the IMX219 in the camera kit with the OV5640. You can build a surround view system using the deserializer board and 4x Ov5640 cameras on AM62P with GPU stitch application.
I'll provide you additional instructions early next week.
Regards,
Jianzhong
Hello Libin,
Have you purchased the OV5640 cameras from Arducam?
Regards,
Jianzhong
Hi Jianzhong,
I contacted Arducam. This is not available yet.
Best regards
Libin Jose
Hi Libin,
Ok. Please open a new thread once you have the cameras. I'll provide a patch to enable 4x OV5640 cameras on AM62P. For now, I'll close this one.
Regards,
jianzhong