Hi Ki,
May you can help me with the next trap:
It seems the compiler doesn't find the definition "ISRAM" which resides in old .tcf or .cdb-file:
Thanks, Wolfgang
P.S.:
I can open .tcf only with editor. There's also a cdb-file in the project. But when trying to open this
(I think it's equal content) I've to specify XDC Tools Root Directory - If I do so, ("C:\noBackup\CCS7\xdctools_3_50_02_20_core")
a Window "ScriptPane" tells me: "Unable to Create BIOS Config Server".
I don't need to edit this. I only need the compiler to make an *.out file :-)