This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625:USB0 does not work intermittently after repeatedly turning it on and off.

Part Number: AM625

Tool/software:

Hi, Team!

I have the same issue as this thread : AM625: AM625 USB0 can only enumerate once as device

I'm having issues with USB0 being recognized, and then once it's not recognized, it won't come back to life no matter how many times I turn it on and off.

The schematic followed the datasheet recommendations,
USB mode is device mode.

As per the thread, I added a 1.2k ohm pull-down resistor to the USB0_VBUS line and the symptom did not appear.

I'm curious if this is the right solution and if TI has done any further research.