This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
I am using the AM625 TI EVK board, which has two Ethernet ports.
When both Ethernet ports are used simultaneously (while checking speed using iperf3), the speed for each port is around 400-500 Mbps. However, when only one port is used at a time, the speed increases to around 800-900 Mbps (almost double).
Can any one tell me what is the reason behind this ?
Hi,
You asked this question on this thread and I answered it. Essentially the network performance is limited by the processing performance of the ARM processors in the device.
Best Regards,
Schuyler