Part Number: AM625
Other Parts Discussed in Thread: , SK-AM62B-P1, SK-AM62-LP, SK-AM62B, SK-AM62-SIP, SK-AM62
Tool/software:
Hi,
We have custom board based on AM625. We pretty much followed AM62-SK(Eval board). Board is not booting. Basically PORZ_OUT is not getting high. We did following checks. Please let me know how to diagnose it further.
1. Checked all voltage rails (3.3_SYS, 1v8_IO,1v8_analog,vddshv_mmc , 1v2, VDD_Core, Vddr_core). All voltages are coming up within the range
2. Checked all PGOOD signals and PGOOD comes high.
2. Checked MCU_OSC0_XI (xin) pin for clock input. Observed clocks comes in within the signal level.
3. Checked MCU_PORz signal. It comes high after all voltage rails gets settled.
4. Checked MCU_RESETz. It comes high.
5.SoC_WARM_RESETz . It comes high.
Still PORZ_OUT is low. As per TRM, if these checks are done, PORZ_OUT should get high to come out of reset.
We even replaced the processor once to check for any assembly issues. Same pattern got observed after replacing the processor. Have taken x-ray for BGA void and everything looks normal. Please let me know is there any debug pin or procedure to findout the issue.
Thanks,
siva.
14
1192
12
12