This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5748: AM5748

Part Number: AM5748
Other Parts Discussed in Thread: SYSBIOS, DP83869HM

Tool/software:

Hi,

We are using custom board with AM5748 running on Sysbios (SDK version: 08_01_00_09). AM5748 EMAC is configured in switch mode.

Two DP83869HM ethernet Phy's are connected through RGMII interface. Two peer devices (laptops) are connected to ethernet PHY's as shown in the below image.

If EMAC and peer devices are configured in 100M mode, ping/communication between two peer devices is successful. If they are configured in 1G mode, ping between two peer devices fails (Switch mode is not working).  

Suggestions would be helpful.

I have also attached the application here.

/**********************************************************************
 ************************* Standard Includes **************************
 **********************************************************************/
#include <xdc/std.h> /* initializes XDCtools */
#include <ti/sysbios/BIOS.h> /* initializes SYS/BIOS */
#include <ti/sysbios/knl/Task.h> /* initializes Task module */
#include <xdc/runtime/IHeap.h>
#include <xdc/runtime/System.h>
#include <xdc/runtime/Error.h>
#include <xdc/cfg/global.h>
#include <ti/board/board.h>
#include <string.h>

#include <ti/sysbios/utils/Load.h> /* To get  CPU load */
#include <ti/drv/uart/UART_stdio.h> /* UART Headers*/

/* CSL Chip Functional Layer */
#include <ti/csl/csl_chip.h>
#include <ti/csl/csl_cpswAux.h>
#include <ti/csl/soc.h>

/* EMAC Driver Header File. */
#include <ti/drv/emac/emac_drv.h>
#include <ti/drv/emac/src/v4/emac_drv_v4.h>

#include <ti/drv/emac/soc/emac_soc_v4.h>

#include <ti/sysbios/family/arm/arm9/Cache.h>

/**********************************************************************
 ************************* User Includes ******************************
 **********************************************************************/

int main()
{
    Task_Params taskParams;
    EMAC_DRV_ERR_E returnValue;
    Board_STATUS boardInitStatus = 0;
    Error_Block eb;
    Error_init(&eb);
    EMAC_HwAttrs_V4 emac_cfg;
    EMAC_OPEN_CONFIG_INFO_T open_cfg;
    EMAC_CHAN_MAC_ADDR_T chan_cfg[APP_EMAC_NUM_CHANS_PER_CORE];
    EMAC_CONFIG_INFO_T cfg_info;
    uint32_t port_num = 0;

    /* Board Initialization*/
    Board_initCfg cfg = BOARD_INIT_UART_STDIO | BOARD_INIT_PINMUX_CONFIG
            | BOARD_INIT_MODULE_CLOCK;
    boardInitStatus = Board_init(cfg);
    if (boardInitStatus != 0)
    {
        UART_printf("Board Initialization failure\n");
        return (0);
    }
    UART_printf("Board Initialization success\n");

    /* Interrupt Crossbar Configuration*/
    CSL_xbarMpuIrqConfigure(CSL_XBAR_INST_MPU_IRQ_92,
                            CSL_XBAR_GMAC_SW_IRQ_RX_PULSE);
    CSL_xbarMpuIrqConfigure(CSL_XBAR_INST_MPU_IRQ_93,
                            CSL_XBAR_GMAC_SW_IRQ_TX_PULSE);

    /* Select RGMII Mode for both the ports GMIIx_SEL = 2 (CTRL_CORE_CONTROL_IO_1)*/
    CSL_FINS(
            ((CSL_control_coreRegs *) CSL_MPU_CTRL_MODULE_CORE_CORE_REGISTERS_REGS)->CONTROL_IO_1,
            CONTROL_CORE_CONTROL_IO_1_GMII1_SEL, 0x02U);
    CSL_FINS(
            ((CSL_control_coreRegs *) CSL_MPU_CTRL_MODULE_CORE_CORE_REGISTERS_REGS)->CONTROL_IO_1,
            CONTROL_CORE_CONTROL_IO_1_GMII2_SEL, 0x02U);

    /*GMAC RESET ISOLATION Enable*/
    CSL_FINS(
            ((CSL_control_coreRegs *) CSL_MPU_CTRL_MODULE_CORE_CORE_REGISTERS_REGS)->CONTROL_IO_2,
            CONTROL_CORE_CONTROL_IO_2_GMAC_RESET_ISOLATION_ENABLE, 0U);
    CSL_FINS(
            ((CSL_control_coreRegs *) CSL_MPU_CTRL_MODULE_CORE_CORE_REGISTERS_REGS)->CONTROL_IO_2,
            CONTROL_CORE_CONTROL_IO_2_GMAC_RESET_ISOLATION_ENABLE, 1U);

    ethernetBufferInit();

    EMAC_socGetInitCfg(port_num, &emac_cfg);

    emac_cfg.port[0].phy_addr = EMAC_CPSW_PORT0_PHY_ADDR;
    emac_cfg.port[1].phy_addr = EMAC_CPSW_PORT1_PHY_ADDR;
    emac_cfg.numPorts = MAX_NUM_EMAC_PORTS;
    emac_cfg.macModeFlags =
            EMAC_CPSW_CONFIG_MODEFLG_GIGABIT | EMAC_CPSW_CONFIG_MODEFLG_FULLDUPLEX;

    EMAC_socSetInitCfg(port_num, &emac_cfg);

    open_cfg.hwAttrs = (void*) &emac_cfg;
    open_cfg.loop_back = 0;
    open_cfg.controller_core_flag = 1;
    open_cfg.max_pkt_size = APP_EMAC_INIT_PKT_SIZE;
    open_cfg.mdio_flag = 1;
    open_cfg.num_of_chans = 1;
    open_cfg.num_of_rx_pkt_desc = 256;
    open_cfg.num_of_tx_pkt_desc = 256;
    open_cfg.p_chan_mac_addr = &chan_cfg[0];
    open_cfg.alloc_pkt_cb = app_alloc_pkt;
    open_cfg.free_pkt_cb = app_free_pkt;


    if (port_num == 0)
    {
        open_cfg.phy_addr = 0x0;
        open_cfg.rx_pkt_cb = (EMAC_RX_PKT_CALLBACK_FN_T*) ethernet_callback1;
        chan_cfg[0].chan_num = 0;
        chan_cfg[0].num_of_mac_addrs = 1;
        chan_cfg[0].p_mac_addr = &macId[0];

    }

    if ((returnValue = emac_open(port_num, &open_cfg))
            == EMAC_DRV_RESULT_OPEN_PORT_ERR)
    {
        UART_printf("main: emac_open failure: %d\n", returnValue);
        return FAILURE;
    }
    else
    {
        UART_printf("main: emac_open success\n");
        cfg_info.rx_filter = EMAC_PKTFLT_ALL; //promisc mode
        cfg_info.mcast_cnt = 0;
        cfg_info.p_mcast_list = NULL;
        emac_config(port_num, &cfg_info);
    }

    emacInitStatus = 1;

    printEMACRegisters();

    Task_Params_init(&taskParams);
    taskParams.priority = 15;
    taskParams.instance->name = "EmacRxPkt";
    Task_create(app_test_task_poll_pkt, &taskParams, NULL);

    /* Start BIOS */
    BIOS_start();

    return 0;
}

Thanks,

Sandeep