Part Number: AM69
Tool/software:
Hi Expert,
I have some questions about the RerDes0 port.
Can Interface Alias only choose one of IPX?
For example, it is advertised in SPEC that it can be made into two sets of PCIe x2
But there is no such IP selection in the Table

EVM is designed as follows
Can these functions be used at the same time?
|
SERDES0 Lanes Mapping Options |
|
|
AM69A Pin Name |
AM69A Functions |
|
|
EVM |
|
SERDES0_RX0/TX0 Lane0 |
PCIe x2 |
|
SERDES0_RX1/TX1 Lane1 |
|
|
SERDES0_RX2/TX2 Lane2 |
PCIe x1 |
|
SERDES0_RX3/TX3 Lane3 |
USB 3.0 |
Thanks
Daniel