This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: Can I trigger in interrupt in I2C if there are no I2C devices connected ?

Part Number: TDA4VH-Q1


Tool/software:

Hello, I would like to test the interrupt triggered in one I2C channel.

My questions are: 

If there are no devices connected to the I2C channel and I request a transmission:

1.- Is that going to trigger an interrupt (assuming all interrupt flags are enabled) ?

2.- Am I going to see a clock signal in the SCL pin so I can verify the baud rate?