Tool/software:
Hi, TI expert!
I have a development environment for am6234, with our own evaluation board.
The software SDK version is PROCESSOR-SDK-LINUX-RT-AM62X-08.06.00.42.
From the image below, it can be seen that otp mmr 31 has 2 bytes used to store magic words.

May I ask which magic words are defined in addition to 0xEBC8 that ROM can recognize? What are the enumeration values for magic words and from which document are they from?

The image is from the following link:
Regards,
Li