Part Number: AM62A3
Other Parts Discussed in Thread: SYSCONFIG, UNIFLASH
Tool/software:
hi TI experts
Now we use norflash memory S28HS512T which is accessed through AM62A3 OSPI interface in our customized board, if using " int32_t Flash_eraseBlk(Flash_Handle handle, uint32_t blockNum) " function( erase 256k) , the used flash block can be erased successfully and user data can be wrote to Nor flash device correctly;
but if use "int32_t Flash_eraseSector(Flash_Handle handle, uint32_t sectorNum) (erase 4K)" function, the erase and write operation will be failed.
in fact, most time we may just modify a few bytes data in one sector; before erasing flash, we can copy one sector data into global buffer , then modify some bytes data according to the data
position offset in the buffer , finally write data stored in buffer to the specified sector area, there is no necessary to erase block area every time ;
so why call the "Flash_eraseSector()" function can`t erase data as expected;