This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM69A: Linux OS in SK - AM69 without setup or environment build in ubuntu.

Part Number: PROCESSOR-SDK-AM69A
Other Parts Discussed in Thread: AM69

Tool/software:

I am using SK -  AM69.

For now, I am using Out of box demo application. Now I want to use Linux on which demo application is built. Without using out of box I want to execute python code to stream imx219 camera without using apps_python folder inside edgeai_gst_app folder.

How to run CV2.imshow using opencv in tisdk-edgeai-image-j784s4-evm.wic.xz flashed into SD card. If separate image file of yocto or any linux file directly to flash to SD card without any build or environment setup . kindly provide link directly like flashing this "tisdk-edgeai-image-j784s4-evm.wic.xz" I want for yocto or linux.

Thanks in Advance ,

Ruban