I have built the kernel 2.6.37 using PSP 4.02.007 for beagleboard xM.
PSP does not include the file system so i tried the demo images of file system from the arago repository.
With these images the kernel is not booting. I think this is beacause the demo filesystem images are buid for kernel version 2.6.32.
Then i tried to build the arago filesystem by following the step given at http://arago-project.org/wiki/index.php/Setting_Up_Build_Environment.
How can i build a filesystem image for the specific kernel 2.6.37 build by PSP.
What file do i need to change and what changes should i make. I am not much familiar with open embedded.
Any help would be Greatful.
Thanks,
Anand