This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J721EXSOMXEVM: Regarding Access of OSPI flash sectors during OSPI boot up mode

Part Number: J721EXSOMXEVM


Tool/software:

Hello Team,

we are using the MCAL package MCUSW_09_00_00_15_CONFIG + ti-processor-sdk-rtos-j721e-evm-09_00_00_02

When we are integrating SBL and tifs.bin from TI and booting from OSPI, as we see below SBL is flashed at offset zero of OSPI , tifs.bin at offset 0x80000 of OSPI and App image at offset of 0x100000 of OSPI , so our doubt if we are accessing these many areas of OSPI then even application also needs some flash area to access it for its operation. In Fls confifuration, the Fls sector address is always start address of OSPI , So OSPI start address overlaps with SBL which already present. In this Case, how to resolve this Issue?

Regards,

Pradeep R