Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: TDA4VH
Tool/software:
Hi TI experts,
We are using tda4vh SDK0902 linux native driver to test the network traffic. It's in switch mode. The network topology is as follows:

The port phy2 is !000Mbps. The network traffic priority of this red line is always higher than that of the blue line. For example, if the blue line is sending 500Mbps of data and 800Mbps of data is being sent from the host port at this time, the blue line's data will drop to 200Mbps, while the red line's 800Mbps will not be affected.
Best regards,
Ruijie