PROCESSOR-SDK-J721S2: J721S2 emmc boot stuck at u-boot, after enter 3 commands it can boot to kernel

Part Number: PROCESSOR-SDK-J721S2

Tool/software:

Hi TI expert

by referring to spracy5.pdf TDA4 Flashing Techniques

I can compile TDA4AL codebase and download the image to eMMC by DFU

however eMMC boot stuck at u-boot , I have to enter 3 commands to let it continue to boot kernel image

TARGET => setenv mmcdev 0

TARGET => setenv bootpart 0

TARGET => boot

how can I eMMC boot to kernel automatically from power on? ( It seems 'saveenv' uboot cmd is disabled )

export TI_TARGET_PROJECT=tisdk-base-image

export MACHINE="j721s2-evm"

yocto-build/scripts

./build_apps_proc.sh

uboot_stuck.log
U-Boot SPL 2024.04-ti-g818c76aed67f (Aug 01 2024 - 19:19:47 +0000)
SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
SPL initial stack usage: 13456 bytes
Trying to boot from MMC1
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Loading Environment from nowhere... OK
init_env from device 17 not supported!
Starting ATF on ARM64 core...

NOTICE:  BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty
NOTICE:  BL31: Built : 16:09:05, Feb  9 2024
I/TC:
I/TC: OP-TEE version: 4.2.0-dev (gcc version 13.3.0 (GCC)) #1 Fri Apr 12 09:51:21 UTC 2024 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: GIC redistributor base address not provided
I/TC: Assuming default GIC group status and modifier
I/TC: SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
I/TC: HUK Initialized
I/TC: Activated SA2UL device
I/TC: Fixing SA2UL firewall owner for GP device
I/TC: Enabled firewalls for SA2UL TRNG device
I/TC: SA2UL TRNG initialized
I/TC: SA2UL Drivers initialized
I/TC: Primary CPU switching to normal world boot

U-Boot SPL 2024.04-ti-g818c76aed67f (Aug 01 2024 - 19:19:47 +0000)
SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
Trying to boot from MMC1
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted


U-Boot 2024.04-ti-g818c76aed67f (Aug 01 2024 - 19:19:47 +0000)

SoC:   J721S2 SR1.0 GP
Model: Texas Instruments J721S2 EVM
Board: J721S2X-PM1-SOM rev E4
DRAM:  2 GiB (effective 16 GiB)
Core:  117 devices, 32 uclasses, devicetree: separate
Flash: 0 Bytes
MMC:   mmc@4f80000: 0, mmc@4fb0000: 1
Loading Environment from nowhere... OK
In:    serial@2880000
Out:   serial@2880000
Err:   serial@2880000
am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA02102 cpsw_ver: 0x6BA82102 ale_ver: 0x00293904 Ports:1
Net:   eth0: ethernet@46000000port@1
Hit any key to stop autoboot:  0
MMC: no card present
mmc_init: -123, time 2002
MMC: no card present
mmc_init: -123, time 2002
** Bad device specification mmc 1 **
MMC: no card present
mmc_init: -123, time 2002
** Bad device specification mmc 1 **
Couldn't find partition mmc 1:2
Can't set block device
MMC: no card present
mmc_init: -123, time 2002
** Bad device specification mmc 1 **
Couldn't find partition mmc 1:2
Can't set block device
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
No FDT memory address configured. Please configure
the FDT address via "fdt addr <address>" command.
Aborting!
Bad Linux ARM64 Image magic!
Scanning for bootflows in all bootdevs
Seq  Method       State   Uclass    Part  Name                      Filename
---  -----------  ------  --------  ----  ------------------------  ----------------
Scanning global bootmeth 'efi_mgr':
MMC: no card present
mmc_init: -123, time 2002
No EFI system partition
No EFI system partition
Failed to persist EFI variables
No EFI system partition
Failed to persist EFI variables
No EFI system partition
Failed to persist EFI variables
  0  efi_mgr      ready   (none)       0  <NULL>
** Booting bootflow '<NULL>' with efi_mgr
Loading Boot0000 'mmc 0' failed
EFI boot manager: Cannot load any image
Boot failed (err=-14)
Scanning bootdev 'mmc@4fb0000.bootdev':
MMC: no card present
mmc_init: -123, time 2002
MMC: no card present
mmc_init: -123, time 2002
MMC: no card present
mmc_init: -123, time 2002
MMC: no card present
mmc_init: -123, time 2002
Scanning bootdev 'mmc@4f80000.bootdev':
No working controllers found
k3-navss-ringacc ringacc@2b800000: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:272
k3-navss-ringacc ringacc@2b800000: dma-ring-reset-quirk: disabled
am65_cpsw_nuss_port ethernet@46000000port@1: K3 CPSW: rflow_id_base: 2
ethernet@46000000port@1 Waiting for PHY auto negotiation to complete......... TIMEOUT !
am65_cpsw_nuss_port ethernet@46000000port@1: phy_startup failed
am65_cpsw_nuss_port ethernet@46000000port@1: am65_cpsw_start end error
am65_cpsw_nuss_port ethernet@46000000port@1: K3 CPSW: rflow_id_base: 2
ethernet@46000000port@1 Waiting for PHY auto negotiation to complete......... TIMEOUT !
am65_cpsw_nuss_port ethernet@46000000port@1: phy_startup failed
am65_cpsw_nuss_port ethernet@46000000port@1: am65_cpsw_start end error
No more bootdevs
---  -----------  ------  --------  ----  ------------------------  ----------------
(1 bootflow, 1 valid)
=> <INTERRUPT>
=> setenv mmcdev 0
=> setenv bootpart 0
=> boot
switch to partitions #0, OK
mmc0(part 0) is current device
SD/MMC found on device 0
Can't set block device
20285952 bytes read in 129 ms (150 MiB/s)
107760 bytes read in 28 ms (3.7 MiB/s)
Working FDT set to 88000000
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
Working FDT set to 88000000
   Loading Device Tree to 000000008fee2000, end 000000008fffffff ... OK
Working FDT set to 8fee2000

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
[    0.000000] Linux version 6.6.32-ti-01301-gdb8871293143-dirty (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240620) #1 SMP PREEMPT Thu Aug  1 19:10:56 UTC 2024
[    0.000000] KASLR disabled due to lack of seed
[    0.000000] Machine model: Texas Instruments J721S2 EVM
[    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002880000 (options '')
[    0.000000] printk: bootconsole [ns16550a0] enabled
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created CMA memory pool at 0x0000000bc8000000, size 896 MiB
[    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x0000000bc8000000..0x0000000bffffffff (917504 KiB) map reusable linux,cma
[    0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 KiB) nomap non-reusable optee@9e800000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a0000000..0x00000000a00fffff (1024 KiB) nomap non-reusable r5f-dma-memory@a0000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a0100000..0x00000000a0ffffff (15360 KiB) nomap non-reusable r5f-memory@a0100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a1000000..0x00000000a10fffff (1024 KiB) nomap non-reusable r5f-dma-memory@a1000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a1100000..0x00000000a1ffffff (15360 KiB) nomap non-reusable r5f-memory@a1100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a2000000..0x00000000a20fffff (1024 KiB) nomap non-reusable r5f-dma-memory@a2000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a2100000..0x00000000a2ffffff (15360 KiB) nomap non-reusable r5f-memory@a2100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a3000000..0x00000000a30fffff (1024 KiB) nomap non-reusable r5f-dma-memory@a3000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a3100000..0x00000000a3ffffff (15360 KiB) nomap non-reusable r5f-memory@a3100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a4000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a4000000..0x00000000a40fffff (1024 KiB) nomap non-reusable r5f-dma-memory@a4000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a4100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a4100000..0x00000000a4ffffff (15360 KiB) nomap non-reusable r5f-memory@a4100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a5000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a5000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a5000000..0x00000000a50fffff (1024 KiB) nomap non-reusable r5f-dma-memory@a5000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a5100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a5100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a5100000..0x00000000a5ffffff (15360 KiB) nomap non-reusable r5f-memory@a5100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node c71-dma-memory@a6000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a6000000..0x00000000a60fffff (1024 KiB) nomap non-reusable c71-dma-memory@a6000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node c71-memory@a6100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a6100000..0x00000000a6ffffff (15360 KiB) nomap non-reusable c71-memory@a6100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node c71-dma-memory@a7000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a7000000..0x00000000a70fffff (1024 KiB) nomap non-reusable c71-dma-memory@a7000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node c71-memory@a7100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a7100000..0x00000000a7ffffff (15360 KiB) nomap non-reusable c71-memory@a7100000
[    0.000000] OF: reserved mem: 0x00000000a8000000..0x00000000a9bfffff (28672 KiB) nomap non-reusable ipc-memories@a8000000
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   [mem 0x0000000100000000-0x0000000bffffffff]
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x000000009e7fffff]
[    0.000000]   node   0: [mem 0x000000009e800000-0x00000000a9bfffff]
[    0.000000]   node   0: [mem 0x00000000a9c00000-0x00000000ffffffff]
[    0.000000]   node   0: [mem 0x0000000880000000-0x0000000bffffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x0000000bffffffff]
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling Convention v1.4
[    0.000000] percpu: Embedded 20 pages/cpu s42920 r8192 d30808 u81920
[    0.000000] Detected PIPT I-cache on CPU0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] CPU features: detected: Spectre-v3a
[    0.000000] CPU features: detected: Spectre-BHB
[    0.000000] CPU features: detected: ARM erratum 1742098
[    0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[    0.000000] alternatives: applying boot alternatives
[    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02880000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),57088k@8m(ospi.rootfs),256k(ospi.phypattern);spi-nand0:512k(ospi_nand.tiboot3),2m(ospi_nand.tispl),4m(ospi_nand.u-boot),256k(ospi_nand.env),256k(ospi_nand.env.backup),98048k@32m(ospi_nand.rootfs),256k@130816k(ospi_nand.phypattern) root=PARTUUID=9fb02314-315d-e14f-afc3-36f382ee3d40 rw rootfstype=ext4 rootwait
[    0.000000] Dentry cache hash table entries: 2097152 (order: 12, 16777216 bytes, linear)
[    0.000000] Inode-cache hash table entries: 1048576 (order: 11, 8388608 bytes, linear)
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 4128768
[    0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[    0.000000] software IO TLB: area num 2.
[    0.000000] software IO TLB: mapped [mem 0x00000000fbfff000-0x00000000fffff000] (64MB)
[    0.000000] Memory: 15268776K/16777216K available (11968K kernel code, 1250K rwdata, 4036K rodata, 2432K init, 502K bss, 590936K reserved, 917504K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[    0.000000]  Trampoline variant of Tasks RCU enabled.
[    0.000000]  Tracing variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 960 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] Root IRQ handler: gic_handle_irq
[    0.000000] GICv3: GICv3 features: 16 PPIs
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000
[    0.000000] ITS [mem 0x01820000-0x0182ffff]
[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @880800000 (flat, esz 8, psz 64K, shr 0)
[    0.000000] ITS: using cache flushing for cmd queue
[    0.000000] GICv3: using LPI property table @0x0000000880040000
[    0.000000] GIC: using cache flushing for LPI property table
[    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000880050000
[    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[    0.000000] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[    0.008415] Console: colour dummy device 80x25
[    0.012989] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[    0.023661] pid_max: default: 32768 minimum: 301
[    0.028419] LSM: initializing lsm=capability,integrity
[    0.033753] Mount-cache hash table entries: 32768 (order: 6, 262144 bytes, linear)
[    0.041531] Mountpoint-cache hash table entries: 32768 (order: 6, 262144 bytes, linear)
[    0.050674] RCU Tasks: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1.
[    0.057943] RCU Tasks Trace: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1.
[    0.065802] rcu: Hierarchical SRCU implementation.
[    0.070701] rcu:     Max phase no-delay instances is 1000.
[    0.076239] Platform MSI: msi-controller@1820000 domain created
[    0.082470] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created
[    0.091900] EFI services will not be available.
[    0.096657] smp: Bringing up secondary CPUs ...
I/TC: Secondary CPU 1 initializing
I/TC: Secondary CPU 1 switching to normal world boot
[    0.109757] Detected PIPT I-cache on CPU1
[    0.109807] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000
[    0.109820] GICv3: CPU1: using allocated LPI pending table @0x0000000880060000
[    0.109856] CPU1: Booted secondary processor 0x0000000001 [0x411fd080]
[    0.109916] smp: Brought up 1 node, 2 CPUs
[    0.139266] SMP: Total of 2 processors activated.
[    0.144072] CPU features: detected: 32-bit EL0 Support
[    0.149326] CPU features: detected: CRC32 instructions
[    0.154608] CPU: All CPU(s) started at EL2
[    0.158791] alternatives: applying system-wide alternatives
[    0.165442] devtmpfs: initialized
[    0.176628] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.186614] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[    0.204262] pinctrl core: initialized pinctrl subsystem
[    0.209959] DMI not present or invalid.
[    0.214320] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[    0.221040] DMA: preallocated 2048 KiB GFP_KERNEL pool for atomic allocations
[    0.228686] DMA: preallocated 2048 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.237023] DMA: preallocated 2048 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.245248] audit: initializing netlink subsys (disabled)
[    0.250872] audit: type=2000 audit(0.160:1): state=initialized audit_enabled=0 res=1
[    0.251096] thermal_sys: Registered thermal governor 'step_wise'
[    0.258798] thermal_sys: Registered thermal governor 'power_allocator'
[    0.264959] cpuidle: using governor menu
[    0.275706] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.282673] ASID allocator initialised with 65536 entries
[    0.298126] platform a000000.dp-bridge: Fixed dependency cycle(s) with /bus@100000/dss@4a00000
[    0.307101] platform 4800000.dsi: Fixed dependency cycle(s) with /bus@100000/dss@4a00000
[    0.315407] platform 4800000.dsi: Fixed dependency cycle(s) with /bus@100000/i2c@2040000/dsi-edp-bridge@2c
[    0.325362] platform a40000.pinctrl: Fixed dependency cycle(s) with /bus@100000/pinctrl@a40000/mcu-cpsw-cpts
[    0.335623] platform 4800000.dsi: Fixed dependency cycle(s) with /bus@100000/dss@4a00000
[    0.343929] platform a000000.dp-bridge: Fixed dependency cycle(s) with /bus@100000/dss@4a00000
[    0.352765] platform 4a00000.dss: Fixed dependency cycle(s) with /bus@100000/dsi@4800000
[    0.361061] platform 4a00000.dss: Fixed dependency cycle(s) with /bus@100000/dp-bridge@a000000
[    0.371516] platform a000000.dp-bridge: Fixed dependency cycle(s) with /dp0-connector
[    0.379586] platform dp0-connector: Fixed dependency cycle(s) with /bus@100000/dp-bridge@a000000
[    0.388758] Modules: 27680 pages in range for non-PLT usage
[    0.388763] Modules: 519200 pages in range for PLT usage
[    0.394960] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[    0.407324] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[    0.413726] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[    0.420660] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[    0.427061] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[    0.433995] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[    0.440396] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[    0.447329] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[    0.454580] k3-chipinfo 43000014.chipid: Family:J721S2 rev:SR1.0 JTAGID[0x0bb7502f] Detected
[    0.463741] iommu: Default domain type: Translated
[    0.468659] iommu: DMA domain TLB invalidation policy: strict mode
[    0.475116] SCSI subsystem initialized
[    0.479133] usbcore: registered new interface driver usbfs
[    0.484757] usbcore: registered new interface driver hub
[    0.490204] usbcore: registered new device driver usb
[    0.495663] pps_core: LinuxPPS API ver. 1 registered
[    0.500739] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.510079] PTP clock support registered
[    0.514196] EDAC MC: Ver: 3.0.0
[    0.517686] scmi_core: SCMI protocol bus registered
[    0.522829] FPGA manager framework
[    0.526342] Advanced Linux Sound Architecture Driver Initialized.
[    0.533017] vgaarb: loaded
[    0.535951] clocksource: Switched to clocksource arch_sys_counter
[    0.542317] VFS: Disk quotas dquot_6.6.0
[    0.546352] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.556609] NET: Registered PF_INET protocol family
[    0.561947] IP idents hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.574757] tcp_listen_portaddr_hash hash table entries: 8192 (order: 5, 131072 bytes, linear)
[    0.583677] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    0.591619] TCP established hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[    0.600308] TCP bind hash table entries: 65536 (order: 9, 2097152 bytes, linear)
[    0.608905] TCP: Hash tables configured (established 131072 bind 65536)
[    0.615793] UDP hash table entries: 8192 (order: 6, 262144 bytes, linear)
[    0.622926] UDP-Lite hash table entries: 8192 (order: 6, 262144 bytes, linear)
[    0.630591] NET: Registered PF_UNIX/PF_LOCAL protocol family
[    0.636730] RPC: Registered named UNIX socket transport module.
[    0.642794] RPC: Registered udp transport module.
[    0.647597] RPC: Registered tcp transport module.
[    0.652400] RPC: Registered tcp-with-tls transport module.
[    0.658002] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.664585] NET: Registered PF_XDP protocol family
[    0.669491] PCI: CLS 0 bytes, default 64
[    0.674174] Initialise system trusted keyrings
[    0.678872] workingset: timestamp_bits=46 max_order=22 bucket_order=0
[    0.685651] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.691772] NFS: Registering the id_resolver key type
[    0.696954] Key type id_resolver registered
[    0.701227] Key type id_legacy registered
[    0.705331] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.712180] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.733390] Key type asymmetric registered
[    0.737579] Asymmetric key parser 'x509' registered
[    0.742592] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[    0.750155] io scheduler mq-deadline registered
[    0.754781] io scheduler kyber registered
[    0.758896] io scheduler bfq registered
[    0.764909] pinctrl-single 4301c000.pinctrl: 13 pins, size 52
[    0.770908] pinctrl-single 4301c038.pinctrl: 11 pins, size 44
[    0.776956] pinctrl-single 4301c068.pinctrl: 72 pins, size 288
[    0.783214] pinctrl-single 4301c190.pinctrl: 1 pins, size 4
[    0.789054] pinctrl-single 11c000.pinctrl: 72 pins, size 288
[    0.795141] pinctrl-single 104200.pinctrl: 20 pins, size 80
[    0.800915] pinctrl-single 104280.pinctrl: 8 pins, size 32
[    0.806984] pinctrl-single a40000.pinctrl: 512 pins, size 2048
[    0.816911] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled
[    0.828573] loop: module loaded
[    0.832481] megasas: 07.725.01.00-rc1
[    0.838235] tun: Universal TUN/TAP device driver, 1.6
[    0.844057] VFIO - User Level meta-driver version: 0.3
[    0.850001] usbcore: registered new interface driver usb-storage
[    0.856505] i2c_dev: i2c /dev entries driver
[    0.861576] sdhci: Secure Digital Host Controller Interface driver
[    0.867905] sdhci: Copyright(c) Pierre Ossman
[    0.872492] sdhci-pltfm: SDHCI platform and OF driver helper
[    0.878627] ledtrig-cpu: registered to indicate activity on CPUs
[    0.884955] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    0.891971] usbcore: registered new interface driver usbhid
[    0.897671] usbhid: USB HID core driver
[    0.902486] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
[    0.911167] optee: probing for conduit method.
I/TC: Reserved shared memory is enabled
I/TC: Dynamic shared memory is enabled
I/TC: Normal World virtualization support is disabled
I/TC: Asynchronous notifications are disabled
[    0.915725] optee: revision 4.2 (12d7c4ee)
[    0.932163] optee: dynamic shared memory is enabled
[    0.941784] random: crng init done
[    0.945325] optee: initialized driver
[    0.950464] NET: Registered PF_PACKET protocol family
[    0.955686] Key type dns_resolver registered
[    0.963476] registered taskstats version 1
[    0.967741] Loading compiled-in X.509 certificates
[    0.979582] ti-sci 44083000.system-controller: ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
[    1.039940] omap_i2c 42120000.i2c: bus 0 rev0.12 at 400 kHz
[    1.046583] pca953x 1-0021: supply vcc not found, using dummy regulator
[    1.053437] pca953x 1-0021: using no AI
[    1.080395] pca953x 1-0020: supply vcc not found, using dummy regulator
[    1.087213] pca953x 1-0020: using no AI
[    1.091790] pca953x 1-0022: supply vcc not found, using dummy regulator
[    1.098605] pca953x 1-0022: using AI
[    1.102895] omap_i2c 2000000.i2c: bus 1 rev0.12 at 400 kHz
[    1.109057] platform 4800000.dsi: Fixed dependency cycle(s) with /bus@100000/i2c@2040000/dsi-edp-bridge@2c
[    1.118976] i2c 2-002c: Fixed dependency cycle(s) with /bus@100000/i2c@2040000/dsi-edp-bridge@2c/aux-bus/panel
[    1.129223] i2c 2-002c: Fixed dependency cycle(s) with /bus@100000/dsi@4800000
[    1.136890] pca953x 2-0020: supply vcc not found, using dummy regulator
[    1.143712] pca953x 2-0020: using no AI
[    1.168290] omap_i2c 2040000.i2c: bus 2 rev0.12 at 400 kHz
[    1.174639] pca953x 3-0020: supply vcc not found, using dummy regulator
[    1.181475] pca953x 3-0020: using no AI
[    1.208271] omap_i2c 2050000.i2c: bus 3 rev0.12 at 400 kHz
[    1.214010] ti-sci-intr 42200000.interrupt-controller: Interrupt Router 125 domain created
[    1.222545] ti-sci-intr bus@100000:interrupt-controller@a00000: Interrupt Router 148 domain created
[    1.231882] ti-sci-intr 310e0000.interrupt-controller: Interrupt Router 227 domain created
[    1.240556] ti-sci-inta 33d00000.msi-controller: Interrupt Aggregator domain 265 created
[    1.251206] ti-udma 311a0000.dma-controller: Number of rings: 48
[    1.258178] ti-udma 311a0000.dma-controller: Channels: 24 (bchan: 0, tchan: 8, rchan: 16)
[    1.267571] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:272
[    1.277461] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled
[    1.284222] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66349100, num_proxies:64
[    1.293623] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[878,128] sci-dev-id:259
[    1.303801] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled
[    1.310559] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66349100, num_proxies:64
[    1.318775] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 230, base_baud = 6000000) is a 8250
[    1.328496] 2880000.serial: ttyS2 at MMIO 0x2880000 (irq = 231, base_baud = 3000000) is a 8250
[    1.337354] printk: console [ttyS2] enabled
[    1.337354] printk: console [ttyS2] enabled
[    1.345852] printk: bootconsole [ns16550a0] disabled
[    1.345852] printk: bootconsole [ns16550a0] disabled
[    1.361796] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
[    1.407955] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    1.417972] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[    1.426251] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
[    1.439120] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[    1.446331] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[    1.452564] pps pps0: new PPS source ptp0
[    1.456731] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:1
[    1.467384] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010c, freq:200000000, add_val:4 pps:0
[    1.476191] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fca100
[    1.476443] mmc0: CQHCI version 5.10
[    1.486324] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fca100
[    1.493262] omap-mailbox 31f82000.mailbox: omap mailbox rev 0x66fca100
[    1.500141] omap-mailbox 31f84000.mailbox: omap mailbox rev 0x66fca100
[    1.523963] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit
[    1.614869] mmc0: Command Queue Engine enabled
[    1.619340] mmc0: new HS400 MMC card at address 0001
[    1.624761] mmcblk0: mmc0:0001 S0J56X 14.8 GiB
[    1.632181]  mmcblk0: p1
[    1.635084] mmcblk0boot0: mmc0:0001 S0J56X 31.5 MiB
[    1.640792] mmcblk0boot1: mmc0:0001 S0J56X 31.5 MiB
[    1.646431] mmcblk0rpmb: mmc0:0001 S0J56X 4.00 MiB, chardev (239:0)
[    1.805881] tps6594-rtc tps6594-rtc.4.auto: registered as rtc0
[    1.811851] tps6594-rtc tps6594-rtc.4.auto: hctosys: unable to read the hardware clock
[    2.196213] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
[    2.203713] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
[    2.211800] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
[    2.219888] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[    3.230392] j721e-pcie 2910000.pcie: PCI host bridge to bus 0000:00
[    3.236718] pci_bus 0000:00: root bus resource [bus 00-ff]
[    3.242219] pci_bus 0000:00: root bus resource [io  0x0000-0xffff] (bus address [0x18001000-0x18010fff])
[    3.251681] pci_bus 0000:00: root bus resource [mem 0x18011000-0x1fffffff]
[    3.258568] pci 0000:00:00.0: [104c:b013] type 01 class 0x060400
[    3.264685] pci 0000:00:00.0: supports D1
[    3.268686] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[    3.274442] pci 0000:00:00.0: reg 0x224: [mem 0x00000000-0x003fffff 64bit]
[    3.281302] pci 0000:00:00.0: VF(n) BAR0 space: [mem 0x00000000-0x00ffffff 64bit] (contains BAR0 for 4 VFs)
[    3.292839] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[    3.300952] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01
[    3.307568] pci 0000:00:00.0: BAR 7: assigned [mem 0x18400000-0x193fffff 64bit]
[    3.314866] pci 0000:00:00.0: PCI bridge to [bus 01]
[    3.319919] irq: no irq domain found for interrupt-controller !
[    3.326041] pcieport 0000:00:00.0: PME: Signaling with IRQ 669
[    3.332066] pcieport 0000:00:00.0: AER: enabled with IRQ 669
[    3.338665] ti-udma 285c0000.dma-controller: Channels: 26 (tchan: 13, rchan: 13, gp-rflow: 8)
[    3.349056] ti-udma 31150000.dma-controller: Channels: 60 (tchan: 30, rchan: 30, gp-rflow: 16)
[    3.361710] spi-nor spi0.0: s28hs512t (65536 Kbytes)
[    3.366726] 7 cmdlinepart partitions found on MTD device 47040000.spi.0
[    3.373357] Creating 7 MTD partitions on "47040000.spi.0":
[    3.378831] 0x000000000000-0x000000080000 : "ospi.tiboot3"
[    3.385005] 0x000000080000-0x000000280000 : "ospi.tispl"
[    3.390850] 0x000000280000-0x000000680000 : "ospi.u-boot"
[    3.396760] 0x000000680000-0x0000006c0000 : "ospi.env"
[    3.402391] 0x0000006c0000-0x000000700000 : "ospi.env.backup"
[    3.408645] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
[    3.414546] 0x000003fc0000-0x000004000000 : "ospi.phypattern"
[    3.426471] spi-nor spi1.0: mt25qu512a (65536 Kbytes)
[    3.431588] 7 fixed-partitions partitions found on MTD device 47050000.spi.0
[    3.438627] Creating 7 MTD partitions on "47050000.spi.0":
[    3.444102] 0x000000000000-0x000000080000 : "qspi.tiboot3"
[    3.450148] 0x000000080000-0x000000280000 : "qspi.tispl"
[    3.455962] 0x000000280000-0x000000680000 : "qspi.u-boot"
[    3.461812] 0x000000680000-0x0000006c0000 : "qspi.env"
[    3.467429] 0x0000006c0000-0x000000700000 : "qspi.env.backup"
[    3.473635] 0x000000800000-0x000003fc0000 : "qspi.rootfs"
[    3.479506] 0x000003fc0000-0x000004000000 : "qspi.phypattern"
[    3.486358] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
[    3.531955] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    3.541968] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[    3.550243] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
[    3.563131] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[    3.570342] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[    3.576536] pps pps0: new PPS source ptp1
[    3.580688] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:1
[    3.595447] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[    3.605357] mmc1: CQHCI version 5.10
[    3.607484] clk: Disabling unused clocks
[    3.620932] ALSA device list:
[    3.623892]   No soundcards found.
[    5.120027] sdhci-am654 4fb0000.mmc: Power on failed
[    5.155623] mmc1: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 64-bit
[    5.183795] EXT4-fs (mmcblk0p1): recovery complete
[    5.189837] EXT4-fs (mmcblk0p1): mounted filesystem 40b39a74-e0a0-4c6f-8c09-5860baef1e2a r/w with ordered data mode. Quota mode: none.
[    5.201937] VFS: Mounted root (ext4 filesystem) on device 179:1.
[    5.208210] devtmpfs: mounted
[    5.212102] Freeing unused kernel memory: 2432K
[    5.216725] Run /sbin/init as init process
[    5.302234] systemd[1]: System time before build time, advancing clock.
[    5.324848] NET: Registered PF_INET6 protocol family
[    5.330417] Segment Routing with IPv6
[    5.334108] In-situ OAM (IOAM) with IPv6
[    5.352921] systemd[1]: systemd 255.4^ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -TPM2 -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK -XKBCOMMON +UTMP +SYSVINIT default-hierarchy=unified)
[    5.384700] systemd[1]: Detected architecture arm64.

Welcome to Arago 2023.10!

[    5.400995] systemd[1]: Hostname set to <j721s2-evm>.
[    5.596594] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
[    5.644066] systemd[1]: Queued start job for default target Multi-User System.
[    5.683116] systemd[1]: Created slice Slice /system/getty.
[  OK  ] Created slice Slice /system/getty.
[    5.705293] systemd[1]: Created slice Slice /system/modprobe.
[  OK  ] Created slice Slice /system/modprobe.
[    5.729144] systemd[1]: Created slice Slice /system/serial-getty.
[  OK  ] Created slice Slice /system/serial-getty.
[    5.752891] systemd[1]: Created slice User and Session Slice.
[  OK  ] Created slice User and Session Slice.
[    5.776222] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[  OK  ] Started Dispatch Password Requests to Console Directory Watch.
[    5.800122] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[  OK  ] Started Forward Password Requests to Wall Directory Watch.
[    5.824047] systemd[1]: Expecting device /dev/ttyS2...
         Expecting device /dev/ttyS2...
[    5.844076] systemd[1]: Reached target Path Units.
[  OK  ] Reached target Path Units.
[    5.864014] systemd[1]: Reached target Remote File Systems.
[  OK  ] Reached target Remote File Systems.
[    5.884005] systemd[1]: Reached target Slice Units.
[  OK  ] Reached target Slice Units.
[    5.904016] systemd[1]: Reached target Swaps.
[  OK  ] Reached target Swaps.
[    5.947093] systemd[1]: Listening on RPCbind Server Activation Socket.
[  OK  ] Listening on RPCbind Server Activation Socket.
[    5.972149] systemd[1]: Reached target RPC Port Mapper.
[  OK  ] Reached target RPC Port Mapper.
[    5.997101] systemd[1]: Listening on Process Core Dump Socket.
[  OK  ] Listening on Process Core Dump Socket.
[    6.020238] systemd[1]: Listening on initctl Compatibility Named Pipe.
[  OK  ] Listening on initctl Compatibility Named Pipe.
[    6.044674] systemd[1]: Listening on Journal Audit Socket.
[  OK  ] Listening on Journal Audit Socket.
[    6.068371] systemd[1]: Listening on Journal Socket (/dev/log).
[  OK  ] Listening on Journal Socket (/dev/log).
[    6.092380] systemd[1]: Listening on Journal Socket.
[  OK  ] Listening on Journal Socket.
[    6.108443] systemd[1]: Listening on Network Service Netlink Socket.
[  OK  ] Listening on Network Service Netlink Socket.
[    6.134669] systemd[1]: Listening on udev Control Socket.
[  OK  ] Listening on udev Control Socket.
[    6.156298] systemd[1]: Listening on udev Kernel Socket.
[  OK  ] Listening on udev Kernel Socket.
[    6.176308] systemd[1]: Listening on User Database Manager Socket.
[  OK  ] Listening on User Database Manager Socket.
[    6.228209] systemd[1]: Mounting Huge Pages File System...
         Mounting Huge Pages File System...
[    6.246372] systemd[1]: Mounting POSIX Message Queue File System...
         Mounting POSIX Message Queue File System...
[    6.272380] systemd[1]: Mounting Kernel Debug File System...
         Mounting Kernel Debug File System...
[    6.292348] systemd[1]: Kernel Trace File System was skipped because of an unmet condition check (ConditionPathExists=/sys/kernel/tracing).
[    6.332021] systemd[1]: Mounting Temporary Directory /tmp...
         Mounting Temporary Directory /tmp...
[    6.353800] systemd[1]: Starting Create List of Static Device Nodes...
         Starting Create List of Static Device Nodes    6.363199] systemd[1]: Starting Load Kernel Module configfs...
m...
         Starting Load Kernel Module configfs...
[    6.400819] systemd[1]: Starting Load Kernel Module drm...
         Starting Load Kernel Module drm...
[    6.444610] systemd[1]: Starting Load Kernel Module fuse...
         Starting Load Kernel Module fuse...
[    6.496586] systemd[1]: Starting Start psplash boot splash screen...
         Starting Start psplash boot splash screen.[    6.506590] fuse: init (API version 7.39)
..
[    6.514944] systemd[1]: Starting RPC Bind...
         Starting RPC Bind...
[    6.536260] systemd[1]: File System Check on Root Device was skipped because of an unmet condition check (ConditionPathIsReadWrite=!/).
[    6.553637] systemd[1]: Starting Journal Service...
         Starting Journal Service...
[    6.587870] systemd[1]: Starting Load Kernel Modules...
         Starting Load Kernel Modules...
[    6.605488] cryptodev: loading out-of-tree module taints kernel.
[    6.613766] cryptodev: driver 1.13 loaded.
[    6.616971] systemd-journald[115]: Collecting audit messages is enabled.
[    6.625114] systemd[1]: Starting Generate network units from Kernel command line...
         Starting Generate network units from Kernel co[    6.636550] systemd[1]: Starting Remount Root and Kernel File Systems...
mmand line...
         Starting Remount Root and Kernel File Systems...
[    6.660678] systemd[1]: Starting Coldplug All udev Devices...
         Starting Coldplug All udev Devices...
[    6.704682] systemd[1]: Started RPC Bind.
[  OK  ] Started RPC Bind.
[    6.725434] systemd[1]: Started Journal Service.
[  OK  ] Started Journal Service.
[    6.736504] EXT4-fs (mmcblk0p1): re-mounted 40b39a74-e0a0-4c6f-8c09-5860baef1e2a r/w. Quota mode: none.
[  OK  ] Mounted Huge Pages File System.
[  OK  ] Mounted POSIX Message Queue File System.
[  OK  ] Mounted Kernel Debug File System.
[  OK  ] Mounted Temporary Directory /tmp.
[  OK  ] Finished Create List of Static Device Nodes.
[  OK  ] Finished Load Kernel Module configfs.
[  OK  ] Finished Load Kernel Module drm.
[  OK  ] Finished Load Kernel Module fuse.
[FAILED] Failed to start Start psplash boot splash screen.
See 'systemctl status psplash-start.service' for details.
[DEPEND] Dependency failed for Start psplas…temd progress communication helper.
[  OK  ] Finished Load Kernel Modules.
[  OK  ] Finished Generate network units from Kernel command line.
[  OK  ] Finished Remount Root and Kernel File Systems.
         Mounting FUSE Control File System...
         Mounting Kernel Configuration File System...
         Starting Flush Journal to Persistent Storage...
[    7.112001] systemd-journald[115]: Received client request to flush runtime journal.
         Starting Apply Kernel Variables...
         Starting Create Static Device Nodes in /dev gracefully...
[  OK  ] Mounted FUSE Control File System.
[  OK  ] Mounted Kernel Configuration File System.
[  OK  ] Finished Flush Journal to Persistent Storage.
[  OK  ] Finished Coldplug All udev Devices.
[  OK  ] Finished Apply Kernel Variables.
[  OK  ] Finished Create Static Device Nodes in /dev gracefully.
         Starting Create Static Device Nodes in /dev...
[  OK  ] Finished Create Static Device Nodes in /dev.
[  OK  ] Reached target Preparation for Local File Systems.
         Mounting /var/volatile...
[    7.393613] audit: type=1334 audit(1709054766.088:2): prog-id=6 op=LOAD
[    7.400646] audit: type=1334 audit(1709054766.096:3): prog-id=7 op=LOAD
         Starting Rule-based Manager for Device Events and Files...
[  OK  ] Mounted /var/volatile.
         Starting Load/Save OS Random Seed...
[  OK  ] Reached target Local File Systems.
         Starting Create Volatile Files and Directories...
[  OK  ] Finished Load/Save OS Random Seed.
[  OK  ] Started Rule-based Manager for Device Events and Files.
[  OK  ] Finished Create Volatile Files and Directories.
[    7.583458] audit: type=1334 audit(1709054766.276:4): prog-id=8 op=LOAD
         Starting Network Name Resolution...
[    7.622967] audit: type=1334 audit(1709054766.316:5): prog-id=9 op=LOAD
         Starting Network Time Synchronization...
         Starting Record System Boot/Shutdown in UTMP...
[  OK  ] Finished Record System Boot/Shutdown in UTMP.
[  OK  ] Found device /dev/ttyS2.
[    7.809448] audit: type=1334 audit(1709054766.504:6): prog-id=10 op=LOAD
[    7.821579] audit: type=1334 audit(1709054766.512:7): prog-id=11 op=LOAD
[    7.836043] audit: type=1334 audit(1709054766.512:8): prog-id=12 op=LOAD
         Starting User Database Manager...
[  OK  ] Started User Database Manager.
[  OK  ] Started Network Time Synchronization.
[  OK  ] Reached target System Time Set.
[  OK  ] Started Network Name Resolution.
[  OK  ] Reached target Host and Network Name Lookups.
[  OK  ] Reached target System Initialization.
[  OK  ] Started Daily Cleanup of Temporary Directories.
[  OK  ] Reached target Timer Units.
[  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[  OK  ] Listening on D-Bus System Message Bus Socket.
         Starting Docker Socket for the API...
[  OK  ] Listening on dropbear.socket.
[    8.443532] audit: type=1334 audit(1709252699.512:9): prog-id=13 op=LOAD
         Starting D-Bus System Message Bus...
[  OK  ] Listening on Docker Socket for the API.
[  OK  ] Started D-Bus System Message Bus.
[    8.599113] dbus-broker-lau[376]: memfd_create() called without MFD_EXEC or MFD_NOEXEC_SEAL set
[  OK  ] Reached target Socket Units.
[  OK  ] Reached target Basic System.
         Starting Avahi mDNS/DNS-SD Stack...
         Starting Print notice about GPLv3 packages...
         Starting IPv6 Packet Filtering Framework...
[    8.801931] CAN device driver interface
         Starting IPv4 Packet Filtering Framework...
         Starting Expand the rootfs partiti…to full size of the boot device....
[    8.872308] audit: type=1334 audit(1709252699.940:10): prog-id=14 op=LOAD
[    8.892007] audit: type=1334 audit(1709252699.940:11): prog-id=15 op=LOAD
         Starting User Login Management...
         Starting Telnet Server...
[    8.924628] k3-dsp-rproc 64800000.dsp: assigned reserved memory node c71-dma-memory@a6000000
[  OK  ] Finished IPv6 Packet Filtering Framework.
[  OK  ] Finished IPv4 Packet Filtering Framework.
[  OK  ] Finished Telnet Server.
[    8.987183] cdns-mhdp8546 a000000.dp-bridge: invalid resource (null)
[  OK  ] Reached target Preparation for Netw[    9.022232] k3-dsp-rproc 64800000.dsp: configured DSP for remoteproc mode
ork.
[    9.049216] mc: Linux media interface: v0.10
         Starting Network Configuration...
[    9.072854] pinctrl-single 4301c068.pinctrl: pin PIN54 already requested by 42110000.gpio; cannot claim for 40200000.tscadc
[  OK  ] Started Avahi mDNS/DNS-SD Stack.
[    9.128546] k3-dsp-rproc 64800000.dsp: local reset is deasserted for device
[  OK  ] Finished Expand the rootfs partition to full size of the boot device..
[    9.159004] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
[    9.168689] pinctrl-single 4301c068.pinctrl: pin-54 (40200000.tscadc) status -22
[    9.176373] pinctrl-single 4301c068.pinctrl: could not request pin 54 (PIN54) from group mcu-adc0-default-pins  on device pinctrl-single
[    9.192381] ti_am3359-tscadc 40200000.tscadc: Error applying setting, reverse things back
[    9.229134] remoteproc remoteproc0: 64800000.dsp is available
[    9.250457] remoteproc remoteproc0: Direct firmware load for j721s2-c71_0-fw failed with error -2
[    9.259405] remoteproc remoteproc0: powering up 64800000.dsp
[    9.265659] remoteproc remoteproc0: Direct firmware load for j721s2-c71_0-fw failed with error -2
[    9.266174] omap_rng 4e10000.rng: Random Number Generator ver. 241b34c
[    9.274587] remoteproc remoteproc0: request_firmware failed: -2
[  OK  ] Started User Login Management.
[    9.313553] videodev: Linux video capture interface: v2.00
[    9.337367] k3-dsp-rproc 65800000.dsp: assigned reserved memory node c71-dma-memory@a7000000
[    9.364652] k3-dsp-rproc 65800000.dsp: configured DSP for remoteproc mode
[    9.378242] k3-dsp-rproc 65800000.dsp: local reset is deasserted for device
[    9.393728] remoteproc remoteproc1: 65800000.dsp is available
[    9.400908] remoteproc remoteproc1: Direct firmware load for j721s2-c71_1-fw failed with error -2
[    9.409872] remoteproc remoteproc1: powering up 65800000.dsp
[    9.411119] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[    9.415620] remoteproc remoteproc1: Direct firmware load for j721s2-c71_1-fw failed with error -2
[    9.447081] remoteproc remoteproc1: request_firmware failed: -2
[    9.447306] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[    9.465929] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
[    9.477242] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[    9.488122] cfg80211: failed to load regulatory.db
[  OK  ] Started Network Configuration.
[  OK  ] Reached target Network.
         Starting containerd container runtime...
[    9.602561] am65-cpsw-nuss 46000000.ethernet eth0: PHY [46000f00.mdio:00] driver [TI DP83867] (irq=POLL)
[  OK  ] Started Netperf Benchmark Server.
         Starting Permit User Sessions...
[    9.661092] am65-cpsw-nuss 46000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[    9.681769] at24 0-0050: supply vcc not found, using dummy regulator
[    9.729871] platform 41000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[    9.764861] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[    9.812813] vdec 4210000.video-codec: Added wave5 driver with caps: 'ENCODE' 'DECODE'
[    9.825137] vdec 4210000.video-codec: Product Code:      0x521c
[  OK  ] Finished Permit User Sessions.
[    9.847773] vdec 4210000.video-codec: Firmware Revision: 320127
[  OK  ] Started Getty on tty1.
[  OK  ] Started Serial Getty on ttyS2.
[  OK  ] Reached target Login Prompts.
         Starting Synchronize System and HW clocks...
[    9.887841] m_can_platform 26a1000.can: m_can device registered (irq=776, version=32)
[    9.897450] platform 41000000.r5f: configured R5F for IPC-only mode
[    9.904054] m_can_platform 40528000.can: m_can device registered (irq=777, version=32)
[    9.921203] m_can_platform 40568000.can: m_can device registered (irq=778, version=32)
[    9.945111] platform 41000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000
[    9.959474] remoteproc remoteproc2: 41000000.r5f is available
[    9.989295] remoteproc remoteproc2: attaching to 41000000.r5f
[   10.031431] gpio-mux mux-controller-0: 2-way mux-controller registered
[   10.040069] platform 41000000.r5f: R5F core initialized in IPC-only mode
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPL-3.0 packages:
        bash
        cifs-utils
        dosfstools
        grub-common
        grub-edite[   10.077815] rproc-virtio rproc-virtio.16.auto: assigned reserved memory node r5f-dma-memory@a0000000
nv
        grub-efi
        kbd-keymaps-pine
        less
        libdw1
        libelf1
        libgcc1
        libreadline8
        libstdc++6
        parted

If you do not wish [   10.098331] virtio_rpmsg_bus virtio0: rpmsg host is online
to distribute GPL-3.0 components please remove
the above packag[   10.109091] m_can_platform 2731000.can: m_can device registered (irq=779, version=32)
es prior to distribution.  This can be done using
the opkg remo[   10.120196] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
ve command.  i.e.:
    opkg remove <package>
Where <package> i[   10.133325] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
s the name printed in the list above

NOTE: If the package is a dependency of another package you
      will be notified of t[   10.153711] rproc-virtio rproc-virtio.16.auto: registered virtio0 (type 7)
he dependent packages.  You should
      use the --force-remova[   10.164537] remoteproc remoteproc2: remote processor 41000000.r5f is now attached
l-of-dependent-packages option to
      also remove the depende[   10.164684] gpio-mux mux-controller-1: 2-way mux-controller registered
nt packages as well
*******************************************[   10.191741] m_can_platform 2751000.can: m_can device registered (irq=780, version=32)
********************
******************************************[   10.206516] platform 5c00000.r5f: configured R5F for remoteproc mode
*********************
[   10.216045] platform 5c00000.r5f: assigned reserved memory node r5f-dma-memory@a2000000
[  OK  ] Finished Print notice about GPLv3 packages.
[   10.236036] remoteproc remoteproc3: 5c00000.r5f is available
[   10.244063] remoteproc remoteproc3: Direct firmware load for j721s2-main-r5f0_0-fw failed with error -2
[   10.253871] remoteproc remoteproc3: powering up 5c00000.r5f
[   10.262904] remoteproc remoteproc3: Direct firmware load for j721s2-main-r5f0_0-fw failed with error -2
[   10.272622] remoteproc remoteproc3: request_firmware failed: -2
[  OK  ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
         Starting Virtual Console Setup...
[   10.771322] m_can_platform 26a1000.can main_mcan16: renamed from can0
[  OK  ] Finished Virtual Console Setup.
[  OK  ] Reached target Hardware activated U[   10.869511] m_can_platform 40528000.can mcu_mcan0: renamed from can1
SB gadget.
[  OK  ] Finished Synchronize System and HW [   10.939387] m_can_platform 2731000.can main_mcan3: renamed from can3
clocks.
[  OK  ] Started containerd container runtime.
[   10.969394] m_can_platform 2751000.can main_mcan5: renamed from can4
[  OK  ] Reached target Multi-User System.
         Starting Record Runlevel Change in UTMP...
[   11.008042] m_can_platform 40568000.can mcu_mcan1: renamed from can2
[   11.028208] [drm] Initialized tidss 1.0.0 20180215 for 4a00000.dss on minor 0
[  OK  ] Finished Record Runlevel Change in UTMP.
[   11.212945] tidss 4a00000.dss: [drm] Cannot find any crtc or sizes
[   11.383338] tidss 4a00000.dss: [drm] Cannot find any crtc or sizes
[   11.719011] tidss 4a00000.dss: [drm] Cannot find any crtc or sizes

 _____                    _____           _         _
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
              |___|                    |___|

Arago Project j721s2-evm ttyS2

Arago 2023.10 j721s2-evm ttyS2

j721s2-evm login: [   12.283972] k3_r5_rproc bus@100000:r5fss@5c00000: Timed out waiting for 5c00000.r5f core to power up!
[   12.296247] platform 5e00000.r5f: configured R5F for remoteproc mode
[   12.302974] platform 5e00000.r5f: assigned reserved memory node r5f-dma-memory@a4000000
[   12.311692] remoteproc remoteproc4: 5e00000.r5f is available
[   12.317531] remoteproc remoteproc4: Direct firmware load for j721s2-main-r5f1_0-fw failed with error -2
[   12.326933] remoteproc remoteproc4: powering up 5e00000.r5f
[   12.332517] remoteproc remoteproc4: Direct firmware load for j721s2-main-r5f1_0-fw failed with error -2
[   12.341899] remoteproc remoteproc4: request_firmware failed: -2
[   14.331965] k3_r5_rproc bus@100000:r5fss@5e00000: Timed out waiting for 5e00000.r5f core to power up!

Switch is changed to DFU mode

j721s2-evm

#  dfu-util -R -a bootloader -D E:\PROJ2\TI_ADAS\EAG_1127\tiboot3.bi

# dfu-util -R -a tispl.bin -D E:\PROJ2\TI_ADAS\EAG_1127\tispl.bin

#  dfu-util -R -a u-boot.img -D E:\PROJ2\TI_ADAS\EAG_1127\u-boot.img

 

TARGET => env default -f -a

TARGET => setenv mmcdev 0

TARGET => setenv bootpart 0

 TARGET => setenv dfu_alt_info ${dfu_alt_info_emmc}

 TARGET => gpt write mmc 0 ${partitions}

TARGET => dfu 0 mmc 0

 

# dfu-util -a tiboot3.bin.raw -D E:\PROJ2\TI_ADAS\EAG_1127\tiboot3.bin

# dfu-util -a tispl.bin.raw -D E:\PROJ2\TI_ADAS\EAG_1127\tispl.bin

# dfu-util -a u-boot.img.raw -D E:\PROJ2\TI_ADAS\EAG_1127\u-boot.img

# dfu-util -a rootfs -D E:\PROJ2\TI_ADAS\EAG_1127\tisdk-base-image-j721s2-evm.rootfs.img

 

TARGET => mmc partconf 0 1 1 1

TARGET => mmc bootbus 0 2 0 0

 

 

2.   Switch is changed to eMMC(boot0) mode

  

TARGET => setenv mmcdev 0

TARGET => setenv bootpart 0

TARGET => boot

  • Hi Yao,

    Can you try adding the following 3 lines to the configs/j721s2_evm_a72_defconfig file in the U-boot folder of SDK,rebuild U-BOOT and try.Theses changes are basically for enabling the save env feature on U-BOOT.In the below patch,it is removing,but for enabling saveenv you will have to add the below 3 lines to the config file.

    Thanks

    Gokul

  • => setenv mmcdev 0
    => setenv bootpart 0
    => saveenv
    Saving Environment to FAT... OK

    after I apply this patch, 'saveenv' works, but It seems the u-boot setting is saved at MMC card FAT. 

    I can auto boot to kernel from power on with microSD card inserted. The auto boot fail when microSD card doesn't exist.

    How to change the A72 u-boot setting to auto boot from eMMC without microSD card ?

    U-Boot 2024.04-ti-g818c76aed67f (Aug 01 2024 - 19:19:47 +0000)

    SoC: J721S2 SR1.0 GP
    Model: Texas Instruments J721S2 EVM
    Board: J721S2X-PM1-SOM rev E4
    DRAM: 2 GiB (effective 16 GiB)
    Core: 117 devices, 32 uclasses, devicetree: separate
    Flash: 0 Bytes
    MMC: mmc@4f80000: 0, mmc@4fb0000: 1
    Loading Environment from FAT... MMC: no card present
    mmc_init: -123, time 2002
    ** Bad device specification mmc 1 **
    In: serial@2880000
    Out: serial@2880000
    Err: serial@2880000
    am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA02102 cpsw_ver: 0x6BA82102 ale_ver: 0x00293904 Ports:1
    Net: eth0: ethernet@46000000port@1
    Hit any key to stop autoboot: 0
    MMC: no card present
    mmc_init: -123, time 2002
    MMC: no card present
    mmc_init: -123, time 2002
    ** Bad device specification mmc 1 **
    MMC: no card present
    mmc_init: -123, time 2002
    ** Bad device specification mmc 1 **
    Couldn't find partition mmc 1:2
    Can't set block device
    MMC: no card present
    mmc_init: -123, time 2002
    ** Bad device specification mmc 1 **
    Couldn't find partition mmc 1:2
    Can't set block device
    libfdt fdt_check_header(): FDT_ERR_BADMAGIC
    No FDT memory address configured. Please configure
    the FDT address via "fdt addr <address>" command.
    Aborting!
    Bad Linux ARM64 Image magic!
    Scanning for bootflows in all bootdevs
    Seq Method State Uclass Part Name Filename
    --- ----------- ------ -------- ---- ------------------------ ----------------
    Scanning global bootmeth 'efi_mgr':
    MMC: no card present
    mmc_init: -123, time 2002
    No EFI system partition
    No EFI system partition
    Failed to persist EFI variables
    No EFI system partition
    Failed to persist EFI variables
    No EFI system partition
    Failed to persist EFI variables
    0 efi_mgr ready (none) 0 <NULL>
    ** Booting bootflow '<NULL>' with efi_mgr
    Loading Boot0000 'mmc 0' failed
    EFI boot manager: Cannot load any image
    Boot failed (err=-14)
    Scanning bootdev 'mmc@4fb0000.bootdev':
    MMC: no card present
    mmc_init: -123, time 2002
    MMC: no card present
    mmc_init: -123, time 2002
    MMC: no card present
    mmc_init: -123, time 2002
    MMC: no card present
    mmc_init: -123, time 2002
    Scanning bootdev 'mmc@4f80000.bootdev':
    No working controllers found
    k3-navss-ringacc ringacc@2b800000: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:272
    k3-navss-ringacc ringacc@2b800000: dma-ring-reset-quirk: disabled
    am65_cpsw_nuss_port ethernet@46000000port@1: K3 CPSW: rflow_id_base: 2
    ethernet@46000000port@1 Waiting for PHY auto negotiation to complete......... TIMEOUT !
    am65_cpsw_nuss_port ethernet@46000000port@1: phy_startup failed
    am65_cpsw_nuss_port ethernet@46000000port@1: am65_cpsw_start end error
    am65_cpsw_nuss_port ethernet@46000000port@1: K3 CPSW: rflow_id_base: 2
    ethernet@46000000port@1 Waiting for PHY auto negotiation to complete......... TIMEOUT !
    am65_cpsw_nuss_port ethernet@46000000port@1: phy_startup failed
    am65_cpsw_nuss_port ethernet@46000000port@1: am65_cpsw_start end error
    No more bootdevs
    --- ----------- ------ -------- ---- ------------------------ ----------------
    (1 bootflow, 1 valid)

  • Hi Novasky,

    Can you try adding the following 3 lines to the configs/j721s2_evm_a72_defconfig file in the U-boot folder of SDK,rebuild U-BOOT and try.Also remove the 3 lines which you had added previously.The below patch saves the environment to eMMC instead of SD.