This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7-Q1: The CSI-TX supports three virtual channels with different resolutions

Part Number: AM62A7-Q1


Tool/software:

HI,

I used an aggregator to merge the two cameras into one MIPI CSI input。

Virtual channel 1 and virtual channel 2 are the image signals input by the OX05B camera, with a resolution of 2592*1944 and a frame rate of 30 FPS.

Virtual channel 3 is the video stream input of the OX03C camera, with a resolution of 1300*670 and a frame rate of 50FPS.

I used MAX96716 aggregator to merge them into the AM62A.

Currently, I am using SDK version 8.6.

Can TI's SDK receive this MIPI CSI data signal?

Thanks

Yuwei Wu