Tool/software:
Dear TI Experts,
We are currently working on enabling communication between the main core (R5/A53) and the HSM core on the AM62x platform. Here are our current plans and questions, and we’d like your guidance to confirm if they are correct:
1. Communication with HSM Core
Current Understanding:
- We have identified the Secure Proxy thread IDs for the HSM core from the TI documentation:
- Write Thread (to HSM):
TISCI_SEC_PROXY_HSM_WRITE_LOW_PRIORITY_THREAD_ID - Read Thread (from HSM):
TISCI_SEC_PROXY_HSM_READ_RESPONSE_THREAD_ID
- Write Thread (to HSM):
- To enable communication with the HSM core:
- Add an entry to
gSciclientMapfor HSM with the corresponding Secure Proxy thread IDs and Host ID (TISCI_HOST_ID_HSM_0). - Update
Sciclient_getCurrentContextto return the HSM context for messages specific to HSM.
- Add an entry to
- Modify the TISCI message header to set the
hostfield toTISCI_HOST_ID_HSM_0for messages targeting the HSM core.
Questions:
- Is this approach to route messages to the HSM core via Secure Proxy correct?
- Are there any additional steps or configurations required to enable communication with the HSM core?
2. Loading Firmware onto the HSM Core
Current Understanding:
- For loading firmware onto the HSM core, we are considering the following options:
- Using the standard
Bootloader_loadCpuAPI as is used for loading regular APP images. - Using
Sciclient_loadFirmwarefromsciclient.c, which seems to be related to firmware management.
- Using the standard
Questions:
- Which method is recommended for loading firmware onto the HSM core?
- If
Sciclient_loadFirmwareis required, could you provide more details on how it should be used specifically for the HSM core?
Your guidance on the above points would be greatly appreciated.
Best regards,
Yang