TDA4VM: Question about PWM module in TDA4

Part Number: TDA4VM

Tool/software:

Hi,TI

The SDK example and the chip manual do not seem to describe the input function of PWM,

Can the PWM module measure the speed based on the speed signal (TDA4_CCR)?

Thanks.

  • I normally think of a PWM as an output. 
    I suppose that you are thinking of using TIMER IO7. If so, the input clock to the timer would typically run anywhere from the crystal frequency to ~250MHz depending upon the selected clock.

    Kevin